how to download s19 file?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to download s19 file?

5,348件の閲覧回数
dreamcatcher
Contributor I
i use tbdml to debug the board.i have the following question when using hiwave.exe to download .s19 file:
1)when load application in hiwave.exe ,it failed,the eeor is:
Error: Syntax:
LOAD [<applicationName>]
     |
     "[<applicationName>]"[CODEONLY|SYMBOLSONLY|AUTOERASEANDFLASH][NOPROGRESSBAR]
     [NOBPT][NOXPR][NOPRELOADCMD][NOPOSTLOADCMD][DELAY]
     [VERIFYFIRST|VERIFYALL|VERIFYONLY][VERIFYOPTIONS|SYMBOLSOPTIONS]

2)when using "load" command, there become the following eeor:

procedure does not exit!

3)can anybody tell me a specific method to download .s19 file.

the corresponding mcu is mc9s12d64

 

 

what's going on?

thanks!

 
 
0 件の賞賛
返信
1 返信

1,151件の閲覧回数
DanielM
Contributor III
dreamcatcher,

what version of CW are you using?

What happens when you click on "TurboBDM HCS12"->"Flash..."? Do you see the flash of the device OK? Can you mark all blocks, erase them and load the S19 from the flash window?

Daniel
0 件の賞賛
返信