can´t install KDS plugin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can´t install KDS plugin

Jump to solution
1,723 Views
lucianonicolau
Contributor III

Hi pgo, I need help,

When install USBDM 4.11.1.60 the folder (...\jre\...) does not exist and it can´t install the USBDM plugins, see the error:

pastedImage_2.png

I tried to install this with no success:

C/C++ Development Tools             x.x.x.xxxxxxxxxxxx

C/C++ GCC Cross Compiler Support    x.x.x.xxxxxxxxxxxx

C/C++ GDB Hardware Debugging        x.x.x.xxxxxxxxxxxx  

C/C++ Memory View Enhancements      x.x.x.xxxxxxxxxxxx

pastedImage_0.png

when install KDS3.0 is it need to install "Eclipse LUNA CDT"?

How can I solve it?

0 Kudos
Reply
1 Solution
1,400 Views
lucianonicolau
Contributor III

Now I solded it, I found the javaw.exe and copying all this folder:

C:\Freescale\KDS_3.0.0\eclipse\features\com.somniumtech.jre.win32.win32.x86_1.7.0.76\jre

and past it as a new folder:

C:\Freescale\KDS_3.0.0\eclipse\jre

then the USBDM installation software can find the folder and install the plugin correctly.

I think the next release will need fix it.

Luciano

View solution in original post

0 Kudos
Reply
2 Replies
1,401 Views
lucianonicolau
Contributor III

Now I solded it, I found the javaw.exe and copying all this folder:

C:\Freescale\KDS_3.0.0\eclipse\features\com.somniumtech.jre.win32.win32.x86_1.7.0.76\jre

and past it as a new folder:

C:\Freescale\KDS_3.0.0\eclipse\jre

then the USBDM installation software can find the folder and install the plugin correctly.

I think the next release will need fix it.

Luciano

0 Kudos
Reply
1,400 Views
pgo
Senior Contributor V

Hi Luciano,

A simpler solution would be to install a java jre from https://java.com/en/download/

I didn't realise this would be a problem as I already have java installed.  The only workaround that seem sensible are:

  • Install a java jre Download Free Java Software
  • Manually add the update site afterwards and manually install the plugins - it's not very complicated but a bit of a nuisance.

Ok - A simple solution: Copy kinetis-design-studio.ini to eclipse.ini or use the new version 4.11.1.70.

The method I'm using to install the plugin seems to be the "suggested method" from the Eclipse project.

bye

0 Kudos
Reply