Wytec USBDM Driver Installation problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wytec USBDM Driver Installation problem

1,429件の閲覧回数
alsimo
Contributor I

I am having a problem installing the driver for the Wytec USBDM. My operating system is Windows XP Professional.

I am using the USBDM_4_9_3_Win Windows Installation Package.

 

When running the installation, it terminates and displays: Cannot Install this Hardware

                                                                                                       

                                                                                                         There is a problem installing the hardware

 

                                                                                                         USBDM BDM Interface

 

                                                                                                         Am error occured during the installation of the device

 

                                                                                                         The parameter is incorrect

 

I have tried this several times with the same results.

 

I also tried installing the driver using zadig_v1.1.1.143 Zadig Application and got:

 

                                                                                                        Driver Installation: FAILED (Invalid parameter)

 

Any help with this would be greatly appreciated. Thanks

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,110件の閲覧回数
pgo
Senior Contributor V

Dear Alsimo,

 

I can only suggest trying to install on a different machine.  I haven't had any error resembling the one you describe.

 

There might be something specific to your machine e.g. language or USB interface that is upsetting the driver install.

 

If you look in the hardware manager does the device appear?  What PID/VID does it have?

 

bye

 

0 件の賞賛
返信