Stand-alone Flash Programmer for TWR-K60N512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stand-alone Flash Programmer for TWR-K60N512

2,796 Views
pozz
Contributor III

Actually I have a tower system based on TWR-K60N512 (Kinetis) processor board. I can program the flash memory of microcontroller through IAR Electronic Workbench, choosing PE Micro/OSJTAG programmer.

 

I couldn't find a stand-alone software (external from IAR IDE) that can only erase/program/verify the microcontroller flash.

 

I found and downloaded/installed USBDM 4.9.3, but the ARM Programmer utility can't find a USBDM programmer. Should I upgrade the firmware from OSBDM to USBDM? How to do that?

 

Another possibility is to use the command line utilities from CodeSourcery Lite, but I don't know if a flash programmer utility is present.

Tags (2)
0 Kudos
Reply
3 Replies

1,408 Views
pgo
Senior Contributor V

Dear Pozz,

 

USBDM and OSBDM are different utilities that do similar things,

 

You can "crossgrade" from OSBDM to USBDM but it requires a HCS08 programmer to reprogram the Kinteis board.  It would also not be supported by Freescale so might invalidate any warranty.

 

USBDM has been tested by me on a K60 board and works OK.  Note however that this is with Codewarrior and the provided USBDM programmer - There is no driver for IAR.

 

bye

0 Kudos
Reply

1,408 Views
pozz
Contributor III

You can "crossgrade" from OSBDM to USBDM but it requires a HCS08 programmer to reprogram the Kinteis board.  It would also not be supported by Freescale so might invalidate any warranty.

 

After flashing USBDM firmware, could I reinstall OSBDM firmware later?

 

USBDM has been tested by me on a K60 board and works OK.  Note however that this is with Codewarrior and the provided USBDM programmer - There is no driver for IAR.

 

Does the stand-alone programmer work?

0 Kudos
Reply

1,408 Views
pgo
Senior Contributor V

 

...

After flashing USBDM firmware, could I reinstall OSBDM firmware later?

Yes - you can download OSBDM image from the P&E web site.

You would need a HCS08 programmer to do so (but you need that anyway).

 

...

Does the stand-alone programmer work?

Yes.

 

bye

0 Kudos
Reply