What can I do to restore the configuration dialogue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What can I do to restore the configuration dialogue

Jump to solution
1,736 Views
changxiushanwu
Contributor II

Once I checked the "don't show this dialogue in future" so the dialogue disappeared.

But now I want to show this dialogue again  What can I do to restore the dialogue?

Tags (2)
0 Kudos
Reply
1 Solution
1,544 Views
pgo
Senior Contributor V

Dear Changxiushanwi,

 

Just try debugging without the BDM connected. 

 

You should get an error dialogue with three options. One of these options being to "Change Settings". 

 

This will open the missing dialogue.

 

Sorry - this is not obvious but I have no other way of doing this in the legay Codewarrior due to how low a level the dialogue operates at.

 

PS. You could also delete the settings file to restore the defaults %APPDATA%/usbdm/usbdm_HC12.cfg.

 

bye

View solution in original post

0 Kudos
Reply
4 Replies
1,544 Views
BlackNight
NXP Employee
NXP Employee

Hello,

the answer might depend on which dialog we are talking about.

Could you tell which dialog you mean?

 

BK

0 Kudos
Reply
1,544 Views
changxiushanwu
Contributor II

Ok,It's this dialogue

I just checked the "don't show this dialogue in future"

0 Kudos
Reply
1,545 Views
pgo
Senior Contributor V

Dear Changxiushanwi,

 

Just try debugging without the BDM connected. 

 

You should get an error dialogue with three options. One of these options being to "Change Settings". 

 

This will open the missing dialogue.

 

Sorry - this is not obvious but I have no other way of doing this in the legay Codewarrior due to how low a level the dialogue operates at.

 

PS. You could also delete the settings file to restore the defaults %APPDATA%/usbdm/usbdm_HC12.cfg.

 

bye

0 Kudos
Reply
1,544 Views
changxiushanwu
Contributor II

Thank you very much.

This is a nice solution.

Thank you for your prompt reply.:smileyvery-happy:

0 Kudos
Reply