What can I do to restore the configuration dialogue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What can I do to restore the configuration dialogue

跳至解决方案
1,740 次查看
changxiushanwu
Contributor II

Once I checked the "don't show this dialogue in future" so the dialogue disappeared.

But now I want to show this dialogue again  What can I do to restore the dialogue?

标记 (2)
0 项奖励
回复
1 解答
1,548 次查看
pgo
Senior Contributor V

Dear Changxiushanwi,

 

Just try debugging without the BDM connected. 

 

You should get an error dialogue with three options. One of these options being to "Change Settings". 

 

This will open the missing dialogue.

 

Sorry - this is not obvious but I have no other way of doing this in the legay Codewarrior due to how low a level the dialogue operates at.

 

PS. You could also delete the settings file to restore the defaults %APPDATA%/usbdm/usbdm_HC12.cfg.

 

bye

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,548 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

the answer might depend on which dialog we are talking about.

Could you tell which dialog you mean?

 

BK

0 项奖励
回复
1,548 次查看
changxiushanwu
Contributor II

Ok,It's this dialogue

I just checked the "don't show this dialogue in future"

0 项奖励
回复
1,549 次查看
pgo
Senior Contributor V

Dear Changxiushanwi,

 

Just try debugging without the BDM connected. 

 

You should get an error dialogue with three options. One of these options being to "Change Settings". 

 

This will open the missing dialogue.

 

Sorry - this is not obvious but I have no other way of doing this in the legay Codewarrior due to how low a level the dialogue operates at.

 

PS. You could also delete the settings file to restore the defaults %APPDATA%/usbdm/usbdm_HC12.cfg.

 

bye

0 项奖励
回复
1,548 次查看
changxiushanwu
Contributor II

Thank you very much.

This is a nice solution.

Thank you for your prompt reply.:smileyvery-happy:

0 项奖励
回复