Using KDS with USBDM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using KDS with USBDM

3,908 Views
gustavsl
Contributor III

Hi, I've managed to install and run KDS with USBDM and configure it successfully. I'm running a Ubuntu Server installation.

However, when I try to run (or debug) an application, there's an error in the final launch sequence:

Error in final launch sequence

Failed to execute MI command:

monitor reset halt

Error message from debugger back end:

"monitor" command not supported by this target.

Failed to execute MI command:

monitor reset halt

Error message from debugger back end:

"monitor" command not supported by this target.

"monitor" command not supported by this target.

I have GDB installed on KDS.

What could it be?

Thanks.

Tags (3)
0 Kudos
Reply
4 Replies

3,350 Views
andrewmeyerbti
Contributor III

In my case I get that all the time when I have too many breakpoints enabled.  Using KE06 chips that is two, and since you need 1 for main . . .    I also get it if one of the breakpoints is not able to be properly set.

0 Kudos
Reply

3,412 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gustavo leal,

Could you tell me the full name of you chip?

What the detail operation system you are using? You can try it in windows 7 system, it can works ok.

You should make sure your USBDM can works in your platform.

About the configuration, you can refer to this link and check it again:

USBDM Functions in Eclipse (including Kinetis Design Studio)

Regards,

Jingjing

0 Kudos
Reply

3,412 Views
gustavsl
Contributor III

Hi. I'm using the MKL26Z64.

I'm running it on a Ubuntu 14.04 server with XFCE.

I managed to partially solve the problem.

One of the libraries required to launch the USBDM ARM GDB Server (libwx_gtk2u-unnoficial) was missing. I installed this library and tcl-8.5 and the GDB server launched.

Now I can flash the chip using the ARM Flash Programmer application, but I still can't do it from inside KDS.

Thanks,

Gustavo.

0 Kudos
Reply

3,412 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gustavo Leal,

    From the kds_user_guide.pdf, it need ubuntu14.04 LTS,

pastedImage_0.png

So, maybe KDS in your ubuntu 14.04 with XFCE will have problem, you should better working in the operation system which KDS defined.

At least, when I working in Window7 ,USBDM can works ok.

Regards,

Jingjing

0 Kudos
Reply