UsbdmFlashProgrammer command line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UsbdmFlashProgrammer command line

1,599件の閲覧回数
wernerdungs
Contributor I

Hi,

I have a problem with UsbdmFlashProgrammer command line.

I use a HCS08 MC9S08PA32 Cpu and want to program it with the UsbdmFlashProgrammer tool.

If the cpu was not programmed before (clean and fresh one) the UsbdmFlashProgrammer commandline failed with BDM_RC_SYNC_TIMEOUT.

If I use the windows version then a messagebox comes out with ' Cycle power'. If I do this (power off the device and power on again) then the programming works.

Also after this point the UsbdmFlashProgrammer commandline works as well.

What can I do that UsbdmFlashProgrammer commandline works also with fresh and clean cpu's ?

Best regards

Werner

0 件の賞賛
返信
0 返答(返信)