Unable to detect microcontroller in CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to detect microcontroller in CodeWarrior

1,009件の閲覧回数
kpro3
Contributor I

I have a KITMMA955XLEVM: Sensor Toolbox for Xtrinsic Smart Sensing Platform, and using CodeWarrior 10.2.

I am trying to create a custom program and load it on to the microcontroller. However, I am unable to connect or even find the microcontroller when attempting to enter debug mode.

osbdm.jpg

I'm running a Bareboard Project with Open Source BDM. The board is connected to the computer through a single USB cable. I am able to use Sensor Toolbox to read the data from the board. The CPU type on the board is MCF51QE64CLH.

I am running on Windows 7 Home Premium 64-bit. I've tried re-installing the drivers from PEMicro.com, but nothing shows up in Device Manager.

osbdm2.jpg.png

Any help or advice would be greatly appreciated. Cheers.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)