USBICP.exe Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBICP.exe Problem

10,818件の閲覧回数
periklis
Contributor I
I have made an OSBDM board. I am trying to programm it for the first time. I installed the drivers for windows sucesfuly. So each time i connect the board to the usb port it is recognized as a motorola device.
The problem is that when i am trying to run usbicp.exe it dosnt do enything. The programm wont start. I am running windows xp_sp2. Can someone help me?
ラベル(2)
タグ(2)
0 件の賞賛
返信
8 返答(返信)

3,606件の閲覧回数
slawko
Contributor I

Hi,

 

I have the same problem like periklis. I used the USBICP.exe some time before and I didnt have any problem just for now. The program do nothing. I try on my other PC with no success. I alsow format my system and load clear XP. Anyone HELP?, PLEASE!!!.

 

 

 

0 件の賞賛
返信

3,606件の閲覧回数
slawko
Contributor I

So... I resolve..... Everyone who the same problem must install a Microsoft Office then USBICP.exe is working. It is not a joke!!! I dont know why but is working with this program. If you uninstall program the problem return. Someone know why???

0 件の賞賛
返信

3,606件の閲覧回数
periklis
Contributor I
It seems that i have a problem with the computer and not with the osbdm board. Every time i run the usbisp.exe it dosnt start. I meen it dosnt do enything. Even when i pressed ctr+alt+del to watch the proceses that are runing i noticed that the usbicp apears only for a second in the proceces window and then it desapears again. I have donload it many times and it has always the same behavior. Tomorrow i will try it on an other computer to see what will hapen.
0 件の賞賛
返信

3,606件の閲覧回数
UcTechnoGeek
Contributor II
I have heard this from other people.
 
It is a computer problem.  Maybe a virus scanner or firewall issue in Windows.  I don't know the exact problem yet, but using a different computer always seems to work.
 
uCTechnoGeek
0 件の賞賛
返信

3,606件の閲覧回数
periklis
Contributor I
I did change the 10nf to 100nf and i still get the same behavior. The device is recognized by windows as a Motorola JB16/JG16 ICP device , but usbicp.exe wont run.
0 件の賞賛
返信

3,606件の閲覧回数
periklis
Contributor I
At the begining i dint had a capacitor on the reset pin. Then my problem was that i couldnt install the windows drivers. Every time i pluged the osbdm in the usb i was geting a fault message. Then i put a 10 nf on the reset pin ( i hadnt read about the 100nf ) and windows found new hardware and i installed the drivers. My problem now is that usbicp.exe dosnt do enything. It dosnt start and i dont get any message. How does the program respond to you if you try to run it whitout having the osbdm pluged into your computer?
I will now try to change the 10nf with a 100nf.

Message Edited by periklis on 2007-04-1509:32 AM

0 件の賞賛
返信

3,606件の閲覧回数
peg
Senior Contributor IV
Hi,
 
I don't have the OSBDM plugges in right now.
If I start USBISP.exe it first shows an Open File dialogue looking for the correct "Personal File" (*.imp)
I choose one.
Then it throws up a very small window complaining Error in calling Open_Device()!
If I OK that it still shows the main window of the programme.
 
What do you get?
 
0 件の賞賛
返信

3,606件の閲覧回数
peg
Senior Contributor IV
Hi periklis,
 
Have you seen this thread:
 
 
Have you a 0.1uf on reset? Do you have oscillations?
 
I have ONLY used the USB software on WinXP SP2.
 
0 件の賞賛
返信