USBDM has problem when program MC9S08PT32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM has problem when program MC9S08PT32

1,884 Views
wangbaode
Contributor IV

Hi pgo,

USBDM has problem when I program MC9S08PT32.

first,USBDM can detect chip ID,but can't find chip type.

pastedImage_0.png

so,I modify the hcs08_device.xml.and  it can find chip type.

pastedImage_0.png

so, I program the chip,but another question comes out.

pastedImage_2.png

Is it OK to use USBDM  to debug MC9S08PTxx?

Tags (1)
0 Kudos
Reply
2 Replies

1,538 Views
pgo
Senior Contributor V

Hi Wang,

I don't have a PT32 to test with.  I tried a PT60 and USBDM had no problems programming my test file.  There isn't much difference between the PT32 & PT60 chips and I have checked the device description in the XML file. I can't suggest any reason for the problem.  I suggest you have another look at the PT32 entry in the XML and see if you can spot any errors (apart from the missing ID #).

Could you try the following:

  • Restore the XML file to the original form
  • Start the programmer
  • Manually choose the PT32 chip from the menu.  Don't use the autodetect as I didn't know the chip ID when adding the PT32 entry.
  • Try programming.

Let me know the error message produced.

bye

0 Kudos
Reply

1,538 Views
wangbaode
Contributor IV

Hi pgo,

I try again and again according to your suggestion. and result is failed.

pastedImage_0.png

I don't know your BDM version.But my BDM version information is as follow:

BDM hardware : USBDM_SWD_SER_JS16CWJ_V2.0

BDM firmware :V4.10.4

USBDM version:V4.10.5

and my test chip is M9S8PT32VLD

0 Kudos
Reply