I have CodeWarrior 10.7, USBDM_4_12_1_180_win and USBDM_Drivers_1_3_0_Win_x64 all on Windows 7 64-bit. With the USBDM connecter the device manager showed "Interface 0 - USBDM' and "USBDM CDC Interface" - both under " Other Devices" and both showed "No Driver Installed". After removing, installing, repairing, reinstalling the driver many times a device eventually appeared under "Debug devices" and it had a driver. I was then able to program my S08SH4 - once. After that - back to square one. Eventually I re-established the device driver and tried to do a firmware upgrade. This worked until I was instructed to "unplug the device, wait a few moments and re-connect the BDM". I then got the message that part 2 of the process had failed. Since then I am unable to load the device driver - so no USBDM.
已解决! 转到解答。
Hi Cox,
I just moved your question from CodeWarrior for MCU space to OSBDM and TBDML space
Thus our USBDM expert would be able to see it.
Jennie Zhang.
Hi Julian,
Can you provide the following information so that I can suggest some things to try:
bye
Hello pgo,
I am using USBDM for MC9S12GA48 microcontroller for programing and debugging. I am using Windows 10 enterprise. My USBDM is based on JM16 design. USBDM is working fine with codewarrior in Win7. I can see the connection in CW5.2 in Win7.
I have installed latest drivers and USBDM in Win 10. I can program my board with HCS Programmer app available in USBDM. But, in CW5.2, I can not see the USBDM in the connection dialog list.
am I missing something?
Thanks and Regards,
Gavali N. K.
Hi pgo
Not sure of the make - it just says "freescale USBDM" on the case, but it does use a JS16 chip.
The good news is that it is now working. I tried loading the driver using the "Update Driver" from the the device driver window and selected the driver myself rather than the automatic option.
The bad news is that CodeWarrior will not select it as debug hardware. In Debug Settings I select the Connection Type "USBDM HCS Interface" and Preferred BDM as "USBDM-JS16-SWD_SER-0001" I get the message : -
Error launching DEO_01_Issue_6_FLASH_PnE U-Multilink
There was an error parsing the memory configuration file
Hi Julian,
It should not be necessary to select anything in the debug settings and, in fact, it's quite hard to create a debug setting from scratch since the debugger startup and memory files depend on the target
If you create a new project with the USBDM interface does the launch configuration look correct?
see USBDM: Codewarrior - Eclipse V10.x
The error message seems to be indicating that it is looking for the wrong kind of interface and/or is missing a memory configuration file which is part of the Target settings
If you try launching without the USBDM plugged in does it complain about a missing BDM?
bye
Just moved onto a different machine with a "clean" windows 7 installation. In the devices window it is shown as "JS16"
I downloaded the driver package "USBDMDrivers_1_3_0_Win_x64.msi" from SourceForge and ran the package.
In Device Manager, under "Hardware Debugging Interfaces" it was listed as "USBDM BDM Interface"
I created a new project named Issue_1_BDM with USBDM Interface. The Connection type is "USBDM HCS08 Interface" under "Connections | Preferred BDM" we have "Any Connected BDM " and under that window it says "Generic BDM"
When I launch Debug The message says "No suitable BDM Module Found"
Also when I launch the HCS08 Programmer it says "No Devices Found"
At no time do I see any Comms activity (the COM light never flashes)
Hi Julian,
I suspect the device is in in-circuit-programming (ICP) mode.
Try the following please:
Bye
Hi Cox,
I just moved your question from CodeWarrior for MCU space to OSBDM and TBDML space
Thus our USBDM expert would be able to see it.
Jennie Zhang.