USBDM_JM60 TBDML errror message

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM_JM60 TBDML errror message

Jump to solution
5,251 Views
raghu123
Contributor I

Hello everyone,

                      i have rigged up the ckt for BDM pod given in USBDM_JM60 distribution, and have tried the download code for hcs12 target (mc9s12dg256) using TBDML. it works well till the selection of the target(we have to manually select the target as TBDML does not identify chip id(0x0033), and the progress bar moves upto 33% and after that i get an error message saying"Error while loading diagnostics alogrithm to Target system.The chip may be secured ,or the derivative selected may be wrong".

 

So if anyone knows solution to this plaese reply.  

     

0 Kudos
Reply
1 Solution
1,751 Views
pgo
Senior Contributor V

Dear Raghu,

 

I've used the USBDM with a similar chip, the MC9S12DG128 without problems.

 

Try running TBDML HCS12->Unsecure.

 

Also check the reset and BKGD signals with a CRO to check if the hardware appears to be working OK.

 

bye

View solution in original post

0 Kudos
Reply
3 Replies
1,751 Views
raghu123
Contributor I

Dear pgo, 

             i have sent the gerber files of the  usbdm  pcb v1.6  for manufacturing , the pcb person says that component values we get printed on the smd pad and will difficult for component mounting. 

 

is there any gerber files for the pcb  which do not have component values on the smd  pads?

0 Kudos
Reply
1,751 Views
pgo
Senior Contributor V

Dear raghu123,

 

Attached are gerber files without component values.

 

bye

 

 

 New Folder.zip

Message Edited by t.dowe on 2009-09-02 03:26 PM
0 Kudos
Reply
1,752 Views
pgo
Senior Contributor V

Dear Raghu,

 

I've used the USBDM with a similar chip, the MC9S12DG128 without problems.

 

Try running TBDML HCS12->Unsecure.

 

Also check the reset and BKGD signals with a CRO to check if the hardware appears to be working OK.

 

bye

0 Kudos
Reply