[USBDM] Can't install JS16 Bootloader driver for initial programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[USBDM] Can't install JS16 Bootloader driver for initial programming

4,329件の閲覧回数
Lumbermatt
Contributor I

Hello,

I'm currently building an USBDM v4.8 (JS16 Minimal version for HCS08/CFv1 targets). I routed the circuit myself from the schematics.

 

When I plug the controller in the USB port, a “JS16” device is detected with Vendor ID 15A2 and Product ID 0038.

I installed the Bootloader GUI (ICP software) from this page: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMO9S08JS16&fpsp=1&tab=Design_Tools_... as explained in the documentation.

 

When I invoke the driver installation wizard with the bootloader driver path ( C:\Program Files\Freescale\JS16 USB Driver\Automatic Bootloader USB Driver ), the wizard claims the it found a driver for the device but couldn’t install it because of following error : File not found.

 

I use Windows 7 x64, maybe this be an issue? Do anybody have any clue what could be the source of this problem?

 

Thanks in advance,

 

ラベル(2)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

3,340件の閲覧回数
superman00
Contributor I

Am I the firmware download mistake?now computer cannot identify chip,i how can use bootloader jsfamily GUI firmware download again.

0 件の賞賛
返信

3,340件の閲覧回数
pgo
Senior Contributor V

Dear All,

 

As Gorlik has indicated,

 

Neither the driver install nor the actual GUI bootloader program appear to work on windows 64-bit.

 

It will be necessary to do the initial programming on a Win32 machine.

 

The USBDM software works on Win64.

 

Sorry!

 

0 件の賞賛
返信

3,340件の閲覧回数
pgo
Senior Contributor V

Dear All,

 

Because of the problems with the Freescale JS16 bootloader running under windows-64bit I have written an alternative bootloader customised for USBDM only.

 

This is available here:

 

https://sourceforge.net/projects/usbdm/files/Version%204.9/1.%20Installation_4_9/

 

This has been tested under windows7-64bit.

 

bye

0 件の賞賛
返信

3,340件の閲覧回数
superman00
Contributor I

hellow  my js16 bdm is also download fir mware computer can not identify say cannot  identify usb device excuse me how to solve

0 件の賞賛
返信

3,340件の閲覧回数
ggorlik
Contributor I

I am not 100% sure but I seem to recall that the package you linked to does not contain a 64-bit driver.

did you try on an XP 32-bit system?

0 件の賞賛
返信