Turbo BDM Light (TBDML) can't connect with MC9S12G128 using Codewarrior for HCS12 v5.1 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Turbo BDM Light (TBDML) can't connect with MC9S12G128 using Codewarrior for HCS12 v5.1 ?

2,766 Views
huuhuynhchi
Contributor III

Hi all,

I want to debug on MC9S12G128 through TBDML but untill now I haven't connected TBDML with MCU using CW for HCS12 v5.1.

I think I lack of driver or something, or Window 7 x64 of mine doesn't support CW v5.1 to debug by TBDML.

If anyone have any ide, please help me.

Thank you very much.

Labels (1)
Tags (1)
2 Replies

2,188 Views
pgo
Senior Contributor V

I believe Freescale has changed over to using OSBDM for all their newer chips.

USBDM (which can pretend to be a TBDML) modifies the device files to add in the TBDML option.

See the description  at the bottom of this page:

USBDM: Troubleshooting USBDM

You could try to do this manually.

bye

2,188 Views
huuhuynhchi
Contributor III

Dear pgo,

Thank you very much :smileyhappy:

0 Kudos
Reply