Hello,
I'm encounting a problem using the MC9S12XEP100 mcu. I tried a lot but did not help.
here list the details.
Environment:
MCU: MC9S12XEP100
IDE: CodeWarrior IDE v5.1
Connections: USBDM
Reproduce:
Connect the MCU to the HI-WAVE debugger through a USBDM device, reset and run it. The program will run away after a period of time, the MCU keeps in running state but cannot be halted.
Description:
GDI: DiExecStop() ==> DI_ERR_NONFATAL
GDI: DiErrorGetMessage() ==> 1
GDI: Error Message ==> Unable to execute command
GDI: Reading From Memory Address: 0x381, count: 1
GDI: DiMemoryRead() ==> DI_OK
GDI: 00
STOPPING
Hope the reply.
Best Regards.
Hi Wankui.
This is USBDM related question.
I would suggest you ask your question to OSBDM and TBDML
The engineers who focus on that space may help.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------