TBDML MAX232

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,951件の閲覧回数
admin
Specialist II

Hi,

 

   Just a short question 

 

 

I'm currently building my TBDML. I have tons of MAX232CPE chips and would like to use one of these to build my TBDML. I know the caps are not the same  1.0uF instead of 0.1uF caps (not sure) but also I think the CPE version is a bit slower. 

 

someone is able to confirm that it should work with 1.0uf capacitor and  a MAX232CPE chip ?

 

Thanks

 

 

0 件の賞賛
返信
1 解決策
1,771件の閲覧回数
peg
Senior Contributor IV

Hello,

 

Any type of MAX232 or similar would be suitable for this purpose.

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,771件の閲覧回数
admin
Specialist II

I used the file here http://forums.freescale.com/freescale/board/message?message.uid=5729#U5729

 

 it use a max232 to put firmware into the TBDML mcu.

 

 

thanks

0 件の賞賛
返信
1,772件の閲覧回数
peg
Senior Contributor IV

Hello,

 

Any type of MAX232 or similar would be suitable for this purpose.

 

0 件の賞賛
返信
1,771件の閲覧回数
pgo
Senior Contributor V

Dear Lyncos,

 

I don't see how a MAX232 is useful for a TBDML.  Do you mean a MON08 programmer?

 

I've  used a MAX232CSE (which is similar) for this OK.

 

bye

Message Edited by pgo on 2010-01-31 10:12 PM
0 件の賞賛
返信