Run USBDM applications in console mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run USBDM applications in console mode

2,154件の閲覧回数
a_cyril
Contributor I

pgo

Hello pgo,

I have a task where I need to use the USBDM applications, specifically FirmwareChanger and JS16_Bootloader in console mode. Unfortunately, I discovered that these applications do not support execution of its functions from the command line. The console mode  is particularly useful for automating test procedures.

Is there a reason these applications were not designed to enable both GUI and console mode? As I also understand, the UsbdmFlashProgrammer application does not have this drawback.

Cyril.

タグ(1)
0 件の賞賛
返信
1 返信

2,018件の閲覧回数
pgo
Senior Contributor V

I did not anticipate the need to run these in console mode.  Reprogramming the BDM is an infrequent event (at least that is what I thought).

Another contributor (Tom Hebb) has added console mode for JS16 bootloader.  This will be incorporated in the next release.

bye

0 件の賞賛
返信