Programming JS16 with USBDM (JM)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming JS16 with USBDM (JM)

2,680件の閲覧回数
dschwertb1
Contributor I

Hi!

This is a follow-up to my post from June https://community.nxp.com/message/669508 

For bypassing the JS16 bootloader, it's important that the addresses FFB8/9/A are written:

FFB8: Flash Block Checksum High Byte

FFB9: Flash Block Checksum High Byte

FFBA: Checksum Bypass

It seems that the USBDM Flash Programmer does not write these.

E.g. this is the content of my s19 file:

S106FFB8D135003C

Written with USBDMs Flash Programmer and read again using USBDM Memory Dump, I get this:

S123FFA0FFFFFFFFFFFFFFFFFFFFFFFFFFFF01ADFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFEAE

Written with a PE Multilink:

S123FFA0FFFFFFFFFFFFFFFFFFFFFFFFFFFF01AEFFFFFFFFFFFFFFFFD13500FFFFFFFFFEA4

The difference AD vs AE is OK. This is the clock trim value.

The checksum is calculated from 0xC400 TO 0xFFAD and 0xFFC0 TO 0xFFFF so the trim value does not affect the checksum.

It seems that the USBDM programmer just ignores anything in this address range. Maybe the Flash Programmer is calculating the trim value and writing just this to this page.

Also, the "Verify Flash" does not find this difference.

Programmer: 4.12.1.140

BDM Firmware 4.12.1

DLL Ver 4.12.1.130

Windows 7 Professional, 64 bit

Regards,

Dietmar

0 件の賞賛
返信
3 返答(返信)

2,221件の閲覧回数
dschwertb1
Contributor I

Hi Peter,

thanks a lot. This works.

I would not expect that the Security setting does affect more than the two bits of 0xFFBF. There's no reason for that.

USBDM need not calculate checksums. These are in the s19 file and not affected from the contents of 0xFFAD to 0xFFC0.

It's controlled by the .prm file. E.g. for a JS16 it has these lines:

CHECKSUM
  CHECKSUM_ENTRY
        METHOD_CRC_CCITT
        INIT    0x8D9D
        OF      READ_ONLY   0xC400 TO 0xFFAD
        OF      READ_ONLY   0xFFC0 TO 0xFFFF
        INTO    READ_ONLY   0xFFB8 SIZE 2
        UNDEFINED 0xff
  END     
END

Regards,

Dietmar

0 件の賞賛
返信

2,221件の閲覧回数
pgo
Senior Contributor V

Hi Dietmar,

I view the 16 bytes including the the BACKDOOR key and such to be part of the same structure.

The following are clearly "security related"

BACKDOOR

FLASH/EEPROM protection

SECURITY byte.

The other data that has appeared in this area is less so.

When I originally wrote the programmer interface I thought it useful to have functionality to set the data for this area independent of the memory image.  If I was doing it again I would probably be more minimalist. These days I usually map the whole area to a C struct and program it from the image.

Perhaps I should name it something else or change it but it's unlikely to happen.

Note if you choose the "Smart" option  then it should use the data from the image if present or  use the programmer settings if not.  This is the option I usually use.

bye

0 件の賞賛
返信

2,221件の閲覧回数
pgo
Senior Contributor V

Hi Dietmar,

I'm sorry I missed your earlier post.

The security region of the flash is treated differently by the programmer.

Have a look at the advanced tab in the stand-alone programmer if you wish to manually set these values.

Alternatively, choose "Image" in the target tab to program as regular Flash.

pastedImage_1.png

pastedImage_1.png

In Codewarrior these options are controlled by the launch configuration.

pastedImage_1.png

pastedImage_1.png

USBDM verifies the flash against these modified values.  It does not ignore the differences.

USBDM does not support calculating flash checksums so this would have to be done in some other fashion.

bye