OSBDM with Visual Basic custom software.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OSBDM with Visual Basic custom software.

1,193 Views
holographl
Contributor I

I'm hoping someone here can help me.

I'm working with the hCS08 processor and need to be able to read and write to the memory on the unit directly.  I have purchased a board that will interface from USB to 6wire BDM but so far all the .dlls or other software is made for Codewarrior.  I really need to be able to use Visual Basic or some other Visual language because of the special job I am doing.

 

Has anyone figured out how to do this yet?  If so can you let me know how so far I am not getting anywhere.

 

Also one other thing if I may ask.  The circuit I am programming actually only has a two pin connection.  Can I just use the Gnd and BKGD pins and not use the other.

 

thanks,

Tags (2)
0 Kudos
Reply
0 Replies