OSBDM - connection problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OSBDM - connection problems

2,825件の閲覧回数
AndreCG
Contributor I

Hello

 

I´m having a problem when I try to use hiwave.

 

When I start a connection to the OSBDM, the USB list that usualy appears here:


dbox.jpg
... doesn't apear anymore.
 

I had everything working last week, then this problem came.

 

The drivers are correctly installed.

 

As show in the testlibusb.exe

 testelib

Does anyone knows what's is going on?

 

Hugs

 

Andrew

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,254件の閲覧回数
fish_yu
Contributor III

I think that you may update your Codewarrior with the last service pack. In it,Your BDM will be supported.At the same time, Please to be attention,You also must copy your old BDM Driver named Opensource.dll,for example codewarrior 6.2 which was installed,You ,firstly,may copy Opensource.dll from codewarrior 6.2 which was installed and paste it to another where you want.Secondly, You may copy the last Opensource.dll to $codewarrior directory$\prog\gdi\ and replace the old Opensource.dll.

At last, You may use your coldwarrior to debug the HCS core and HC core. But if you want to debug ColdFire V1 Core,Please copy the old Opensource.dll to $codewarrior directory$\prog\gdi\ and replace the last Opensource.dll.If you need more help,Please continue to post.

0 件の賞賛
返信