Need to (re)program MC9S08 with an embedded linux SoC on the same board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need to (re)program MC9S08 with an embedded linux SoC on the same board

3,234 次查看
Orlopeor
Contributor I

Hello,

I'm new here and I was trying to look for a similar problem, but it seems you are always using or a tool kit or the PC to use ICP in the microcontrollers. Our idea:

We are trying to program your MC9S08 through our embedded Linux SoC, just simulating the BDM protocol lines from the DEMO9S08SH8/SG8 with our GPIOs replacing the BKGD and RESET lines. Do you know where can I get any driver to do this in an embedded Linux? We've already programmed the Freescale's uC with Code Warrior and the kit in our board and it's working, but now we want to be prepared for possible firmware updates using our SoC with embedded linux OS. Is that possible?

Thanks in advance!

Regards


标记 (2)
0 项奖励
回复
1 回复

990 次查看
Orlopeor
Contributor I
Another question:

What happens if we use the I2C signals in order to write in the FLASH memory the .S19 file we got with the Code Warrior?

Thanks!
0 项奖励
回复