Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux

5,933 Views
ben106
Contributor I
Hi,
is it possible to program the microcontroller with Linux ? (I mean Linux on the computer, not on the microcontroller)

And if so, is "live debugging" possible ?

Thanks

Ben
Tags (2)
0 Kudos
Reply
4 Replies

2,470 Views
AceMax
Contributor I

Raise it again!

 

Same question.

0 Kudos
Reply

2,470 Views
greg_b
Contributor I

For now use a virtual machine like VirtualBox.

 

The osbdm-jm60 is an open source driver, sonner or later someone will rewrite it for the GNU/Linux.

0 Kudos
Reply

2,470 Views
admin
Specialist II

Hi

 

I am very interested in doing the same thing. Here is a link which may or may not be usefull:

 

http://www.sparetimelabs.com/funwith08/funwith08.html

0 Kudos
Reply

2,470 Views
BradR
Contributor I
I see that this question has never been answered, so I'd like to raise it again. Is there any support under Linux for the OSBDM08?

Failing that, is there source code available for the PC end of the OSBDM08? I've looked in this forum but so far haven't found any links to the OSBDM08 software. It's possible that a port to Linux would be straightforward.

Message Edited by Brad R on 2008-12-12 10:41 AM
0 Kudos
Reply