JS16 OSBDM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JS16 OSBDM

1,471 次查看
Michael_Theisse
Contributor I

Hallo,

 

refering to USBDM_SOIC_JS16(Minimal):

 

Is it right that BKGD_DRV is connected to input- and output pins on MC9S08JS16CWJ. BKGD_DRV drives only an input pin on U1B (74LV125AD)?

标记 (2)
0 项奖励
回复
1 回复

649 次查看
pgo
Senior Contributor V

Dear Michael,

 

The connections are correct.

 

The two pins are used as outputs to control the buffer at different times with the other pin 3-state.  Neither is actually used as an input.

 

This allows for faster manipulation of multiple port pins on a shared port but also allows independent control using a separate pin.

 

bye

 

0 项奖励
回复