hi pgo,
I meets two questions through USBDM to debug MKE04Z128VLK4.
1,when i use ARM programmer to detect chip,MKE04Z128VLK4 is not a member of the result. result only contains MKE04Z8 and MKE04Z64.
and chip ID is 4280040.
2,when i use codewarrior to debug MKE04Z128,a error dialog comes out.
I think it's a new question.
Solved! Go to Solution.
Hi Wang,
there is an error in the arm_device.xml file. Please find the entry for MKE04Z128M4 and change the 1st two digits of the sdid value to match the one your quoted.
e.g.
<sdid value="0x04000000" /> |
(only the 1st two digits are used 04 => MKE04xxx)
Let me know if this works for both cases.
bye
Hi Wang,
Thanks, I'll update the installation file.
I'm a bit puzzled as the PA60 is meant to have an ID of 0x0000. It looks like there is actually a bug causing it to use the PT60 ID which it is aliased to.
bye
Hi Wang,
there is an error in the arm_device.xml file. Please find the entry for MKE04Z128M4 and change the 1st two digits of the sdid value to match the one your quoted.
e.g.
<sdid value="0x04000000" /> |
(only the 1st two digits are used 04 => MKE04xxx)
Let me know if this works for both cases.
bye
Hi pgo,
according to your suggestion. I change the sdid value as 0x04280040. USBDM works well.ARM programmer can detect MKE04Z128VLK4,and codewarrior can debug the chip through USBDM.
but USBDM still can't debug PA60.can i change sdid like MKE04Z128 to detect PAxx?
thanks.
hi pgo,
according to the way of MKE04Z128VLK4,I open hcs08_device.xml and find the entry of PT60.
I find the <sdid value="0x2040" />.but according to detected result,the id of pA60 is 0x4040.so I update the sdid as 0x4040.
I retry to detect MC9S08PA60.It's surprising that USBDM can detect pt60 and codewarrior can debug the chip.
so I think it's a mistake.could you recorrect the errors for a new version.
bye