Help Building PC executables (dll and test programs)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help Building PC executables (dll and test programs)

ソリューションへジャンプ
3,214件の閲覧回数
osorakunakamori
Contributor I

First, let me offer huge praises to pgo and all other contributers who have done this fantastic work. Thanks so very much!

 

I want to build the PC-side programs of USBDM, namely the dll and test program. What do I need for this? I am guessing Eclipse and cygwin ... is this correct? Has anybody built them with VC++? Any advice to help a stranded newbie is much appreciated!!

 

Thanks! 

  

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,252件の閲覧回数
pgo
Senior Contributor V

Dear osoraku,

 

The DLL for USBDM were built with eclipse & MINGW.   It should be possible to to build them with VC++ but there are some environment variables that should be set for the different targets.  This is done as part of the eclipse setup and would be automatically done if the eclipse packages were imported into Eclipse.

 

bye

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,253件の閲覧回数
pgo
Senior Contributor V

Dear osoraku,

 

The DLL for USBDM were built with eclipse & MINGW.   It should be possible to to build them with VC++ but there are some environment variables that should be set for the different targets.  This is done as part of the eclipse setup and would be automatically done if the eclipse packages were imported into Eclipse.

 

bye

 

0 件の賞賛
返信