HCS12 PROGRAMMER failed to read s-File

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS12 PROGRAMMER failed to read s-File

3,484 Views
wojinandawei
Contributor II

I'M using USBDM 4.12.1.240.

My MCU is MC9SG128.

I want to use HCS12 programmer to programme my mcu, but when load hex file, it tells me "Failed to read S-File".

But when I load S19 files in "USBDM 4.12.1.240\DeviceData\HCS12", it read well.

So,why this happen, what should I do to get through thi situation.

Please help.

Thanks a lot.

0 Kudos
Reply
2 Replies

3,293 Views
wojinandawei
Contributor II

I have solved this issue .

The reason that programmer can't read my *.s19 file is this:

   the s19 file must be placed in the direction(C:\Program Files (x86)\pgo\USBDM 4.12.1.240\DeviceData\HCS12).

After place the file well, the the programmer read it correctly.

0 Kudos
Reply

3,293 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Your issue related with USBDM, please move your question here

https://community.nxp.com/community/bdm 

Thanks

Jennie Zhang

0 Kudos
Reply