HCS08 Flash Programmer for USBDM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS08 Flash Programmer for USBDM

44,141 Views
pgo
Senior Contributor V

Dear All,

 

Attached is a stand-alone Flash programming utility for HCS08 devices.

 

Features
  • Command line usage is available for batch files.
  • GUI usage is available for interactive use.
  • Supports most HCS08 chips (Paged memory is not supported).
  • Trimming of internal target clock to specified frequency.
  • Programming of security options to leave the chip unsecured or secured after programming.
  • May be used to unsecure chips (by mass erase).
  • The code has been written in a modular fashion. It should be straightforward to re-use the flash programming code to create other custom programming utilities.

 

I have tested it on a range of devices and I have found no (more) bugs.  However, no guarantees are given!

 

bye

 

1. Installation_1_0_3.zip

2. Source_1_0_3.zip

Message Edited by t.dowe on 2009-12-08 09:28 AM
Tags (2)
0 Kudos
Reply
46 Replies

1,421 Views
osorakunakamori
Contributor I

Dear pgo,

 

Thanks for your response. You are right, I was referring to CF v1.

 

Thanks again for all the great work.

 

 

0 Kudos
Reply

1,421 Views
Obetz
Contributor III

Nice work!

 

Does it use the new USBDM 2.0 API? Can it be used with OSBDM?

 

Oliver

0 Kudos
Reply

1,421 Views
pgo
Senior Contributor V

Dear Obetz,

 

It uses the new USBDM V2 API so isn't usable with the earlier versions.

 

Sorry!

 

I'll consider back-porting it later but there are other things that should be done first (e.g. paged addressing) and I would like to try improving the clock trimming accuracy.

 

bye

 

0 Kudos
Reply

1,421 Views
Obetz
Contributor III

Hello pgo,

 

thanks for the fast reply.

 

One more question: I don't see any options for the target supply voltage selection, do you intend to use the target supply present in the JM based hardware?

 

This would be very convenient for batch programming.

 

Oliver

0 Kudos
Reply

1,421 Views
pgo
Senior Contributor V

Dear Obetz,

 

The usual USBDM dialogue will open to configure the the target voltage etc. even if using a batch file.

 

However, there is a crude workaround.  The dialogue now contains an option to "not ask again" i.e. the dialogue will not re-appear. You have to delete the config file to restore the dialogue!

 

Your suggestion is very good.  I will add options to control the target power when I have time.

 

bye
Message Edited by pgo on 2009-12-15 02:00 PM
0 Kudos
Reply