Hello,
i'm newbie here so pls be tolerant..
I haveHC9S12C64 Motorola MCU and i'd like to load the serial monitor too via trubo BDM v1.1 programmer. I use this hardware http://img155.imageshack.us/i/dscf7524i.jpg/
Uploaded with [URL=http://imageshack.us]ImageShack.us[/URL]
Have downloaded HCS12SerialMon2r1.abs form freescale forum. But i can not properly load the monitor to MCU. At the end of programming CodeWarrior show me this :
http://img845.imageshack.us/i/20110310193838.jpg/
and after this programming, serial monitor is not working in my MCU,
PLS HELP, Regards
Dear CyccPL,
The image posted is very hard to read!
The only error that I can see is that it can't find "main" to set a breakpoint. This is not surprising since I believe there is no main symbol in the monitor code - its assembly language. It's trying to set a temporary breakpoint at the C main() function.
Use the memory window to check if a file has actually been programmed to the target flash. For example, have a look at $FFFE to see if there is a reset vector & then check at the vector destination to see if there is some code there. This will, at least, indicate if somthing has been programmed to the chip. Of course, its possible that this may be the existing code! You could erase the chip and re-try to be absolutely sure.
Also, You could download the entire monitor program project from Freescale and use that rather than just the abs file. This should program with less hassle.
Search for HCS12SerialMon in the above search box.
Procedure:
Finally - Why do you want to use the monitor anyway? Development using TBDML is much less painful.
bye
Dear pgo..
i have CODE in .s19 filme, and solution for this CODE say that i must load the MONITOR to MCU via BDM, and then UPload the .s19 code via COM to MCU using loaded monitor...
I also try to load the monitor like you said. I download and load project in codewarrior. This time it's flash MONITOR with non errors [movie]. But i still can not put the .s19 code in too MCU. MONITOR is not working, MCU is inaccessible
Mayby MCU can be damaged ?? Pls advice
movie with flasing monitor