BeeKit Export and Import into CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BeeKit Export and Import into CodeWarrior

1,508件の閲覧回数
ChrisRodgers
Contributor I

I'm trying to work through the BeeKit example from BKWCTKUG.pdf from the following lnk:

 

http://cache.freescale.com/files/rf_if/doc/user_guide/BKWCTKUG.pdf?fsrch=1&sr=1

 

I'm using BeeKit 2 and CodeWarrior 10.2 (Special Edition) from the following link:

 

http://cache.freescale.com/lgfiles/devsuites/MCU/CW_MCU_v10.2_SE.exe?WT_TYPE=IDE%20-%20Debug,%20Comp...

 

As per Section 2.6 on page 35, I'm able to Export the solution.

 

But when I open CodeWarrior and try to Import (as per Section 2.7.1 on pg. 36) I am unable to do so.

 

I get the message "No projects found to import"

 

It doesn't say exactly what type of file it's looking for, but it doesn't find it. I can see that there are .XML files but maybe it's looking for something else?

 

If I can't import these files into CodeWarrior, I can't load them into my ZigBEE NCB and SRB units for testing.

 

Any suggestions?

 

Thanks!

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,314件の閲覧回数
HJKIM
Contributor I

You can import the project using CodeWarrior 6.2.0

0 件の賞賛
返信