Hi,
Several days ago, CrasyCat offers a new License.dat of "CW5.0 for 08 SE", then OpenSourceBDM can write FLASH of target MCU. Thanks a lot for CrazyCat.

Now, I happened a new problem on using OSBDM. My procedure is below:
1. Connect a MCU which has a blank FLASH to OSBDM; Run Hiwave 5.0 for 08;
2. "set gdi", then Hiwave can read target's FLASH, obviously, it's blank. And I can reset target too.
3. "Load...", I download a *.s19 file to target FLASH, it's OK! Then in Memory Window of Hiwave, we can read bytes in target FLASH. And, the target MCU can run correctly!
4. When I connect the above target MCU to OSBDM again, some error happened.
I can't erase target MCU's FLASH, FLASH operation error message is "flash module is bad or protected."
5. Then I unsecure the target FLASH follow the "ReadMe_unsecure.txt" file. After several seconds, "Command Windows" show that "done,...". Maybe, the target have been unsecured. But, in fact, the "4. " error happened again...
So, is anyone can solve the problem? If my procedure is fault?
Thanks!
Message Edited by lemonmeng on 04-15-200603:41 AM