9S12XDP512CAG-9S12XDT512CAA dump Address How to fill in

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

9S12XDP512CAG-9S12XDT512CAA dump Address How to fill in

353 次查看
dage_liao
Junior Contributor I

Hi, I want to extract a FLASH&EEPROM backup from 9S12XDP512CAG and 9S12XDT512CAA. How should I enter the address in the USBDM memory dump

0 项奖励
回复
1 回复

340 次查看
pgo
Senior Contributor V

Hi,

It's ages since I've looked at this chip so the following is from a quick inspection of the manual.

Refer to the memory map Figure 1-3. S12X CPU & BDM Global Address Mapping and boundaries in Table 1-2. Device Internal Resources.

Linear address:

[EEPROM_LOW to 0x13_FFFF] => [0x13_F000 to 0x13_FFFF]

[FLASH_LOW to 0x7F_FFFF] => [0x78_0000 to 0x7F_FFFF] 

Attached is a config file to try.

If loading with the HC12 programmer select linear image before loading the file.

bye

0 项奖励
回复