Compatibility of Raspberry pi Official 7 inch LCD With NavQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatibility of Raspberry pi Official 7 inch LCD With NavQ

5,400件の閲覧回数
nilz
Contributor II

Hi,

Is the Raspberry pi Official 7 inch LCD compatible with NavQ? Can you also specify any adapter for external supply to the NavQ with connected peripherals (keyboard, etc.)?  

I appreciate any help you can provide.

Best,

Nilanjan

0 件の賞賛
返信
2 返答(返信)

5,322件の閲覧回数
iaingalloway
NXP Employee
NXP Employee

For powering external peripherals - beyond what the on board USB-C power supply can handle - you can use a powered USB hub. That will offload the power of a keyboard and mouse to the powered hub adapter.

If you are asking how to power the NavQ, then you can use a USB-C input for power. or apply up to 20V on the power input connector header.

see https://nxp.gitbook.io/8mmnavq

 

 

0 件の賞賛
返信

5,322件の閲覧回数
iaingalloway
NXP Employee
NXP Employee

Emcraft have a 7" LCD that has been tested with NavQ. 
Technically many other displays can be made to work, but they have not been tested or had the settings configured for them.

0 件の賞賛
返信