NXP Training Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Training Content

Discussions

Sort by:
This session will focus on the wearable reference design for healthcare and explain design challenges, architecture and technical system details. Subject matter experts from Freescale and hardware and software partners will be on hand to demonstrate an i.MX- and Kinetis-based design. Presented by: aleguzman Presented at: FTF 2014 Session ID: FTF-HCR-F0083
View full article
Learn how an image flows through an i.MX 6 series or i.MX5x applications processor from the sensor, through the image processing unit (IPU), all the way to the display. Learn to set up and control the image path, as well as where the BSP and Uboot must be touched to effect changes. This session will include an instructor-led demonstration based on i.MX 6 series applications processors and homework. Presented by: Oliver Brown Presented at: FTF 2014 Session ID: FTF-CON-F0119
View full article
Are you ready for kernel 3.10.53? Learn how to boot with the device tree, understand bindings and syntax today. Presented by Massimo Bonazzi Presented at DwF Istanbul and Ankara - May 12 and 14, 2015 Session ID: EUF-DES-T1465
View full article
This session will introduce i.MX 6 series hardware design reference board and will walk through the i.MX 6 series SDP schematic. The session will also introduce hardware design consideration including the hardware checking list to facilitate the hardware design and development. Additionally i.MX6D/Q/DL/Solo power design and how to use DDR calibration will be covered. At the end of session, will share the experience of i.MX 6 hardware bring up. Presented at DwF Kinetis MCUs Based on ARM® Technology - Tianjin - 19 March 2015 Session ID: APF-DES-T1023
View full article
Freescale processors have long been utilized for aerospace and defense applications. This session will describe the most commonly selected devices from the i.MX applications processor family, Qorivva portfolio and the QorIQ platform with Layerscape architecture. A Freescale applications engineer will share successful approaches for improving robustness and safety and mitigating system failures for aerospace environments. The session will also summarize the design collateral and support resources available to simplify the certification process. Presented by Pierre Juste Presented at DwF Ankara - May 14, 2015 Session ID: EUF-SNT-T1469
View full article
The news of the past year hasn’t been encouraging for those who wished cyberspace would avoid becoming a geopolitical battleground. It is now confirmed that national governments are exploiting weaknesses in network infrastructure and end point security to conduct cyber surveillance and disrupt the operations of networks and other critical infrastructure. But with QorIQ platforms, embedded systems designers can do more than throw up their hands and surrender. QorIQ products include features like secure boot, which OEMs can use to make it significantly harder for their systems to be hacked. This session will briefly describe the threats which the Trust Architecture is intended to address and provide an overview the features and methods it uses to resist hacks. Presented by Geoff Waters Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1041
View full article
Introduce Freescale high-performance and high integrated MCU products for bootloader. Presented by David Chen Presented at DwF Taipei - May 7, 2015 Session ID: APF-DES-T1456
View full article
Presented by James Huang Presented at DwF Hsinchu
View full article
This session will show how to obtain i.MX technical information from Freescale's website and also give an overview on i.MX 6 series SoC features, including IPU, VPU, GPU, and corresponding i.MX 6 series hardware design reference boards. The session will also show how to use Android® BSP for i.MX 6 series processors KK4.4.2_1.0.0-ga, i.MX 6 series for Linux® BSP fsl-yocto-3.10.17_1.0.0-ga and manufacturing tools. At the end of this session, we will do a few case studies on i.MX 6 series, i.e. multiple camera capturing, dashboard demo, multi-panel display. Presented at DwF Kinetis MCUs Based on ARM® Technology - Tianjin - 19 March 2015 Session ID: APF-DES-T1021
View full article
Presented by Bill Zheng Presented at DwF RF Solutions - Wuhan - 13 August 2015
View full article
Lecture including a live demo, showing how to develop multimedia application for i.MX applications processors, taking advantages of the hardware multimedia accelerators of the i.MX SoC.  Presented by Daniele DallAcqua Presented at DwF Istanbul - May 12, 2015 Session ID: EUF-DES-T1474
View full article
This session will explain how the IoT will change healthcare. Subject matter experts from Freescale and software partners will discuss the One Box reference platform and how it can be used to enable the IoT for healthcare applications. Special attention will be paid to hardware design, communication protocols and the security structure. Presented by: David Niewolny Presented at: FTF 2014 Session ID: FTF-HCR-F0195
View full article
This session will introduce the i.MX series product for Automotive application, such as roadmap, production feature, etc. It will also include i.MX automotive solutions, such as Surround View, Virtual Cluster, etc. Presented at DwF MCU Solutions - Zhengzhou - 31 March 2015 Session ID: APF-ACC-T0990
View full article
This hands-on session will detail how to build portable and diagnostic devices using the Kinetis ARM® Cortex®-M0 and Cortex-M4 products from Freescale. Special attention will be paid to the integration of sensors and Bluetooth® low energy. Presented by: aleguzman Presented at: FTF 2014 Session ID: FTF-HCR-F0197
View full article
This session will help attendees to choose their wireless solution for healthcare by explaining the different options and making recommendations. Special attention will be paid to the Continua Health Alliance for healthcare device interoperability. This hands-on session will allow attendees to implement both an NFC and a BLE solution using the low-cost Freescale Freedom development platform for Kinetis L series MCUs built on the ARM® Cortex®-M0+ processor. Presented by: aleguzman Presented at: FTF 2014 Session ID: FTF-HCR-F0196
View full article
Presented at DwF Kinetis MCUs Based on ARM® Technology - Wuhan - May 27, 2015
View full article
Presented by Bruce Tsai Presented at DwF Hsinchu
View full article
Microcontroller Solutions Enabling multi product development across wide range of price performance points Reduction in cost of SW ownership Faster time to market with hardware & software solutions tightly integrated Services & support NXP Microcontrollers Kinetis & LPC MCUs. Smart. Secured. Secure, Connected. Smart Increasing performance, reducing space & power budgets to deliver more power efficient & intelligent edge node processing Secure Delivering scalable security across the families to facilitate secure edge node processing at right price/performance rations Connected Providing all key wired & in-home wireless connectivity backbones while facilitating reduced cost of ownership for
View full article