NXPトレーニングコンテンツ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Training Content

ディスカッション

ソート順:
Presented by Geoff Lees and John Dixon Presented at DwF Silicon Valley - March 26, 2015
記事全体を表示
In this hands-on session, the low-power consumption features and advantages of Freescale KL series MCU will be introduced in-depth, and attendees will learn how to configure the MCU to enter low-power mode, and how to implement the low-power ADC function by practicing on the KL26 target board. Attendees will also learn how to use FreeMASTER (a free tool from Freescale) to monitor and display the running program on the MCU. Presented at DwF MCU Solutions - Zhengzhou - 31 March 2015 Session ID: APF-IND-T1022
記事全体を表示
Presented by Embedsky Presented at DwF Kinetis MCUs Based on ARM® Technology - Guangzhou - June 10, 2015
記事全体を表示
For 20 years, Freescale has established networking IP and expertise with PowerQUICC and QorIQ processors based on Power Architecture®  technology. In this session, we will discuss the addition of the LS1 family of ARM®-based processors to the QorIQ portfolio and where we are growing the Power Architecture-based portfolio. We will also provide an update on the innovative Layerscape architecture platform and product roadmap for QorlQ LS series. Presented by Lidong Liu Presented at DwF Digital Networking - Nanjing - 21 May 2015 Session ID: APF-SNT-T1046
記事全体を表示
The asymmetric multicore processors provide a solution where a core can run an operating system benefiting from many existing resources, such as Linux. In contrast, the other core enables a real-time control through a preparation for firmware such as MQX™ (RTOS). In this hands-on, in a few hours the participant will have an overview of how to use the asymmetric multicore approach (AMP) offered by SoC VF61 (ARM® Cortex®-A5 + ARM Cortex-M4) with Freescale Vybrid processors. Using a computer-based module in this architecture, the development stages will be explored, from the preparation of the environment to the communication between cores at the application level. Presented by Toradex Presented at DwF IoT Multicore Technologies and Enablement Software Solutions Porto Alegre - 19 March 2015 Session ID: LAT-IND-T1018
記事全体を表示
Presented by Jerry Zeng Presented at DwF Kinetis MCUs Based on ARM® Technology Nanjing - 12 March 2015
記事全体を表示
Presented by ZLG Presented at DwF Kinetis MCUs Based on ARM® Technology - Wuhan - May 27, 2015 & Guangzhou - June 10, 2015
記事全体を表示
Presented at DwF IoT Wireless Module Solutions - Wuhan - May 28, 2015
記事全体を表示
Presented by Tiefeng Shi Presented at DwF RF Solutions - Chengdu - 9 April 2015
記事全体を表示
This session covers two linked topics. The fist part will cover the overview of the new QorIQ LS1 product line. The second portion of the session will explore the key considerations for designing a robust power supply distribution network for the new LS1021A QorIQ processor family. Using the new LS1021A boards as our case study, we will review key factors such as efficiency, design simplification, and Power System Management techniques that are used on the boards and discuss how they are used and why. This session will provide you with a basic understand of key concepts when designing your power supply distribution network. Presented by Sharad Khanal at Linear Technology & Satoshi Iida at Freescale Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1040
記事全体を表示
Freescale QorIQ based access point/router is a complete production-ready, Bill of Materials (BOM)-optimized solution that can support single- or dual-radio 802.11 a/b/g/n/ac devices through MiniPCI or Mini PCI Express® interfaces.  Presented by Jason Wang Presented at DwF Taipei - May 7, 2015 Session ID: APF-SNT-T1460
記事全体を表示
Learn practical methods to integrate video and graphical elements together in your user interface that runs on the i.MX 6 series. The session starts with an introduction of the i.MX 6 series video and graphics hardware components, along with their Linux® OS software libraries. It will then show simple methods to create portable user interface applications, supported by several useful software code examples. Presented by: Daniele Dall'acqua Presented at: FTF 2014 Session ID: FTF-CON-F0223
記事全体を表示
Learn about the wide range of Freescale Made For iPod (MFi) solutions for audio and non-audio accessories and app-based accessories. The solutions are based on Freescale MCUs, MPUs, sensors and analog products, and include software and rapid prototyping hardware systems. This session also includes a range of live audio and non-audio accessory demonstrations. Presented by: Rudan Bettelheim Presented at: FTF 2014 Session ID: FTF-CON-F0019
記事全体を表示
Presented at DwF RF Solutions - Wuhan
記事全体を表示
Presented by Gemotech Presented at DwF Kinetis MCUs Based on ARM® Technology - Tianjin - 19 March 2015
記事全体を表示
The Kinetis Software Development Kit (KSDK) is an extensive set of robust peripheral drivers, communication stacks, middleware and sample applications designed to simplify and accelerate the development in any Kinetis MCU. The addition of Processor Expert technology for software support and board configuration provides ease of use and unmatched flexibility. The Kinetis SDK is free and includes full source code under an open-source permissive license  for all hardware and software abstraction of peripheral drivers. Presented by Denis Shimizu Presented at DwF IoT Multicore Technologies and Enablement Software Solutions - Porto Alegre - 19 March 2015 Session ID: LAT-DES-T1019
記事全体を表示