NXPトレーニングコンテンツ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Training Content

ディスカッション

ソート順:
Learn about Freescale's latest Kinetis and i.MX devices plus view the roadmap offerings. Presented by Dong Sun Presented at DwF Kinetis MCUs Based on ARM® Technology - Guangzhou - June 10, 2015 Session ID: APF-INS-T1013
記事全体を表示
Internet of Things nodes are using a wide plethora of heterogeneous wireless connectivity protocols such as: IEEE® 802.15.4, Thread, ZigBee®, 6LoWPAN/IPv6, and BLE. By attending this session you will learn which wireless communication protocol is the right solution for their application requirements, while comparing various communication protocols for 2.4 GHz and sub-1 GHz technologies. This session will provide an overview on commonly used wireless technologies and standards for smart homes and which Freescale microcontroller families are best suited for connected appliance, sensor device or hub product idea. Presented by Antonio Concio Presented at DwF Istanbul/Ankara - May 12/14, 2015 Session ID: EUF-IND-T1462
記事全体を表示
This session will provide a demonstration of a software-defined networking (SDN) use case that highlights an open vSwitch implementation on QorIQ T4/T2 processors in the cloud with fog/edge nodes using QorIQ P10xx- and T10xx-based gateways. The demonstration will show fail over, load balancing and multi-tenancy. Presented by Sam Siu Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1054
記事全体を表示
This workshop is a superset of the FTF-SDS-F0176 lunch and learn, Xtrinsic Sensor Fusion on Kinetis MCUs. It adds theory of operation for accelerometer, magnetometer and gyroscope. It also provides a fundamental understanding of sensor fusion topics, dives into details of the sensor fusion library and then provides hands-on exploration of the library interfaces. Presented by: Mike Stanley Presented at: FTF 2014 Session ID: FTF-CON-F0178
記事全体を表示
The i.MX 8QuadXPlus Multisensory Enablement Kit (MEK) is a NXP development platform based on Cortex A-35 + Cortex-M4 cores. Built with high-level integration to support graphics, video, image processing, audio, and voice functions, the i.MX 8X processor family is ideal for safety-certifiable and efficient performance requirements. This tutorial shows how to enable the Cortex-M4 using the MCUXpresso SDK package and loading the binary from the network. NOTE: It is also possible to load the Cortex-M4 image from the SCFW using the imx-mkimage utility. Please see next blog posts for this tutorial. Setting up the machine NOTE: This shows the procedure for a Linux environment. For the Windows OS, please see the Getting Started documentation on the SDK package. Install cmake on the host machine: $ sudo apt-get install cmake Download the armgcc toolchain from here :https://launchpad.net/gcc-arm-embedded/5.0/5-2016-q2-update/+download/gcc-arm-none-eabi-5_4-2016q2-20160622-linux.tar.bz2  and export the location as ARMGCC_DIR: $ export ARMGCC_DIR=<your_path_to_arm_gcc>/gcc-arm-none-eabi-5_4-2016q2/ NOTE: The ARMGCC_DIR variable needs to be exported on the terminal used for compilation. To setup the TFTP server on the host machine, follow the first two sections on this blog post https://imxdev.gitlab.io/tutorial/How_to_boot_Kernel_and_File_System_from_the_network/ (Configuring your Host PC for TFTP and Configuring your Host PC for NFS). Downloading the SDKPermalink Download the MCUXpresso SDK following these steps: Click on “Select Development Board”; Select MEK-MIMX8QX under “Select a Device, Board, or Kit” and click on “Build MCUXpresso SDK” on the right; Select “Host OS” as Linux and “Toolchain/IDE” as GCC ARM Embedded; Add “FreeRTOS” and all the wanted Middleware and hit “Request Build”; Wait for the SDK to build and download the package. Building the image All demos and code examples available on the SDK package are located in the directory <<SDK_dir>>/boards/mekmimx8qx/. This tutorial shows how to build and flash the hello_world demo but similar procedures can be applied for any example (demo, driver, multicore, etc) on the SDK. To build the demo, enter the armgcc folder under the demo directory and make sure that the ARMGCC_DIR variable is set correctly. $ cd ~/SDK_2.3.0_MEK-MIMX8QX/boards/mekmimx8qx/demo_apps/hello_world/armgcc $ export ARMGCC_DIR=<your_path_to_arm_gcc>/gcc-arm-none-eabi-5_4-2016q2/ Run the build_release.sh script to build the code. $ ./build_release.sh NOTE: If needed, give the script execution permission by running chmod +x build_release.sh. This generates the M4 binary (hello_world.bin) under the release folder. Copy this image to the /tftpboot/ directory on the host PC. NOTE: This procedure shows how to build the M4 image that runs on TCM. To run the image from DDR, use the build_ddr_release.sh script to build the binary under the ddr_release folder. Flashing the image Open two serial consoles, one for /dev/ttyUSB0 for Cortex-A35 to boot Linux, and one for /dev/ttyUSB1 for Cortex-M4 to boot the SDK image. On the A35 console, with a SD Card with U-Boot, stop the booting process and enter the following commands to load the M4 binary to TCM: => dhcp => setenv serverip <ip_from_host_pc> => tftp 0x88000000 hello_world.bin => dcache flush => bootaux 0x88000000 Then the M4 core will load the image to the /dev/ttyUSB1 console.    
記事全体を表示
With the price per bit of hard disk drive storage continuing to fall, large capacity drives are now available at prices accessible to many consumers. This has led to the growth in popularity of “personal cloud” solutions where the drive is attached to the home wired or wireless network and acts as a central store or back-up system for the devices in the home, known as “consumer Network Attached Storage” or cNAS. This session will introduce the QorIQ LS1024A dual-core communication processor and the optimized cNAS solution offered with this device and used in products such as the WD MyCloud and Synology DS414j. Presented by Jim Bridgwater Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T0979
記事全体を表示
Presented by James Huang Presented at MCU and Automotive Solutions, Tianan - 19 March 2015
記事全体を表示
Introduce sensor hub and fusion solutions, and update the latest sensor product and roadmap.  Presented by Eric Wu Presented at DwF Taipei - May 7, 2015 Session ID: APF-INS-T1457
記事全体を表示
Freescale QorIQ networking devices employ complex packet processing engines, capable of protocol header processing, traffic shaping, prioritization and forwarding without CPU intervention. The offloading capabilities are boosting the performance in traffic forwarding and termination scenarios. Adding also a very large and flexible feature set, the offloading technologies require complex hardware initialization sequences and complex run-time programming techniques.This seminar presents the troubleshooting workflow, the tools and techniques, the counters and other tips that make networking issues investigation easier on both QorIQ eTSEC and DPAA platforms. The main scenarios covered include no connectivity, partial packet loss or performance loss (due to imbalanced CPU processing, kernel upgrades or firmware upgrades). Presented by Du Chen Presented at DwF Digital Networking - Nanjing - 21 May 2015 Session ID: APF-SNT-T1361
記事全体を表示
In this session, we will review the new features available on the QorIQ T4240/T4160 processors. We will cover the new power management features, HiGig, Interlarken, PCI Express® Gen 3 and Data Path Acceleration Architecture (DPAA) enhancements. After completion of this session, you will be more familiar with the new features and should be able to perform the basic debug task with these blocks. Presented by Sam Siu Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1039
記事全体を表示
This session will highlight the differences between the two architectures from the programming model, including overall architecture, instruction set architecture (ISA) and exception handling. After completion of this session, participants should have a good understanding of what is common and how to go about programming with devices based on ARM and Power Architecture technology. Presented by Satoshi Iida Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1043
記事全体を表示
Automotive and Connected Car Design, Software and Services Healthcare and Wearables Smart Industry Insight and Innovation Smart Home and Buildings Smart Networks
記事全体を表示
Automotive and Connected Car Smart Industry Smart Cities Smart Networks
記事全体を表示
This session will introduce the consumer and industry analog products including MMPF0100/200 Power Management Integrated Circuit (PMIC) and describe the new strategy on selling our existing automotive analog products within this industry field.  Presented by Stephen Yan Presented at DwF Kinetis MCUs Based on ARM® Technology - Guangzhou - June 10, 2015 Session ID: APF-IND-T1015
記事全体を表示
This session will address how S12 MagniV mixed-signal MCUs can help customers design more compact and cost-effective electronic control units. The S12 MagniV devices are built on proven S12 technology, enabling software and tool compatibility across the entire portfolio. With the right blend of digital programmability and high-precision analog, plus a portfolio of scalable memory options, the S12 MagniV portfolio streamlines automotive design. Presented at DwF MCU Solutions - Zhengzhou - 31 March 2015 Session ID: APF-ACC-T0982
記事全体を表示
New high-performance WLAN access point, router and gateway solutions addressing the latest IEEE® 801.11ac MU-MIMO features, including a preview of Inteop 2015 demo and add-on service support (AIS based metrics). Presented by Jim Bridgwater Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1049
記事全体を表示
This session will provide am overview of the new automotive MCUs from Freescale, with a particular emphasis on the aspects which allow to reduce BOM or the development cost. The MCU based in ARM® Cortex® architecture and the solutions which allow the possibility to integrate power supply, logic and actuation will be presented. Presented by Lorenzo Daniele Presented at DwF Istanbul - May 12, 2015 Session ID: EUF-ACC-T1466
記事全体を表示
Presented at DwF Kinetis MCUs Based on ARM® Technology - Wuhan - May 27, 2015
記事全体を表示
Smart Networks QorIQ SDN Service Switch Solution
記事全体を表示
Share design experience on Freescale i.MX applications processors. Presented by Jim Lin Presented at DwF Taipei - May 7, 2015 Session ID: APF-SHB-T1452
記事全体を表示