NXPトレーニングコンテンツ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Training Content

ディスカッション

ソート順:
This session covers two linked topics. The fist part will cover the overview of the new QorIQ LS1 product line. The second portion of the session will explore the key considerations for designing a robust power supply distribution network for the new LS1021A QorIQ processor family. Using the new LS1021A boards as our case study, we will review key factors such as efficiency, design simplification, and Power System Management techniques that are used on the boards and discuss how they are used and why. This session will provide you with a basic understand of key concepts when designing your power supply distribution network. Presented by Sharad Khanal at Linear Technology & Satoshi Iida at Freescale Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1040
記事全体を表示
With the price per bit of hard disk drive storage continuing to fall, large capacity drives are now available at prices accessible to many consumers. This has led to the growth in popularity of “personal cloud” solutions where the drive is attached to the home wired or wireless network and acts as a central store or back-up system for the devices in the home, known as “consumer Network Attached Storage” or cNAS. This session will introduce the QorIQ LS1024A dual-core communication processor and the optimized cNAS solution offered with this device and used in products such as the WD MyCloud and Synology DS414j. Presented by Jim Bridgwater Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T0979
記事全体を表示
The session will introduce Kinetis MCUs for supporting Thread and embedded platform as well as provide Alljoyn, HomeKit services through MQX.  Presented by James Huang Presented at DwF Taipei - May 7, 2015 Session ID: APF-SHB-T1454
記事全体を表示
Freescale processors have long been utilized for aerospace and defense applications. This session will describe the most commonly selected devices from the i.MX applications processor family, Qorivva portfolio and the QorIQ platform with Layerscape architecture. A Freescale applications engineer will share successful approaches for improving robustness and safety and mitigating system failures for aerospace environments. The session will also summarize the design collateral and support resources available to simplify the certification process. Presented by Pierre Juste Presented at DwF Ankara - May 14, 2015 Session ID: EUF-SNT-T1469
記事全体を表示
Freescale's Digital Networking products (e.g., QorIQ, QorlQ Qonverge, C29x and Layerscape architecture) incorporate a high-performance cryptosecurity engine called the SEC. In this session, we provide a brief overview of the SEC hardware capabilities, then cover the SEC's programming model, virtualization capabilities and supporting enablement in the SDK, including the SEC Descriptor RunTime Assembler, use within Linux® kernel and user space for IPsec and SSL. Examples will be provided for QorIQ and the C29x public key co-processor. The SEC enablement roadmap for the SDK will also be discussed. Presented by Geoff Waters Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1008
記事全体を表示
Presented at DwF Kinetis MCUs Based on ARM® Technology - Wuhan - May 27, 2015
記事全体を表示
Learn about the fundamentals of DDR, compare DDR4 to DDR3 and discover the new pins and features of DDR4 in QorIQ products. This session will also provide guidelines on hardware and software implementations for DDR4 using QorIQ products. Presented by Garry Guske Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1044
記事全体を表示
The news of the past year hasn’t been encouraging for those who wished cyberspace would avoid becoming a geopolitical battleground. It is now confirmed that national governments are exploiting weaknesses in network infrastructure and end point security to conduct cyber surveillance and disrupt the operations of networks and other critical infrastructure. But with QorIQ platforms, embedded systems designers can do more than throw up their hands and surrender. QorIQ products include features like secure boot, which OEMs can use to make it significantly harder for their systems to be hacked. This session will briefly describe the threats which the Trust Architecture is intended to address and provide an overview the features and methods it uses to resist hacks. Presented by Geoff Waters Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1041
記事全体を表示
Design, Software and Services Accelerating Firmware Development of Kinetis MCUs by using the New Peripheral Drives, Stacks and Middleware of Kinetis SDK Hands-On Workshop: MQX™ RTOS and Kinetis Software Development Kit (SDK) Integration   Smart Industry Hands-On Workshop: Introduction to the Development of Embedded Systems with Asymmetric Multicore Approach Networking Applications with Yocto Project™ Operation Presenting the New QorIQ LS1 MPUs for IoT, M2M
記事全体を表示
Ethercat, Profinet, PROFIBUS, CAN, RS232, etc. are extensively used in communications networks in factories, buildings, transport infrastructures and monitoring/control equipment in our cities. Technologies such as EtherCAT, PROFINET and EtherNet/IP are testament to this. In this session, we will explore how QorIQ LS1 processor families can help equipment manufacturers span this landscape using a QUICC Engine (QE) controller for UART/Ethernet-based protocol implementation, an Enhanced Triple Speed Ethernet Controller (eTSEC) for intelligent Ethernet classification and 2-port switching, and an eight-port gigabit Ethernet switch for wire-rate switching. Further we will look on how QorIQ LS1 family meet the emerging Internet of Things (IoT) requirements as also as the Broadband Home router and NAS market. Presented by Gino Gatto Presented at DwF Istanbul and Ankara- May 12 and 14, 2015 Session ID: EUF-SNT-T1468
記事全体を表示
Freescale is the best positioned silicon maker for the Internet of Tomorrow. This session is all about how Freescale sees the mechanics of the IOT. Attend this session and see what runs under the hood! Presented by Massimo Bonazzi Presented at DwF Istanbul and Ankara - May 12 and 14, 2015 Session ID: EUF-IND-T1463
記事全体を表示
New high-performance WLAN access point, router and gateway solutions addressing the latest IEEE® 801.11ac MU-MIMO features, including a preview of Inteop 2015 demo and add-on service support (AIS based metrics). Presented by Jim Bridgwater Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1049
記事全体を表示
This session will be discuss Layerscape devices, their differentials, software and tools available and examples of applications Presentation by Bruno Castelucci Presented at DwF IoT Multicore Technologies and Enablement Software Solutions - Porto Alegre - 19 March 2015 Session ID: LAT-IND-T1017
記事全体を表示
Yocto Project will be presented, discussing its characteristics, differential and its basic architecture. At the end there will be a demonstration with a QorIQ LS1 board running an image generated by the Yocto Project platform. Read more: www.yoctoproject.org, freescale.github.io Presentation by O.S. Systems Partner Presented at DwF IoT Multicore Technologies and Enablement Software Solutions - Porto Alegre - 19 March 2015 Session ID: LAT-IND-T1017
記事全体を表示
For 20 years, Freescale has established networking IP and expertise with PowerQUICC and QorIQ processors based on Power Architecture®  technology. In this session, we will discuss the addition of the LS1 family of ARM®-based processors to the QorIQ portfolio and where we are growing the Power Architecture-based portfolio. We will also provide an update on the innovative Layerscape architecture platform and product roadmap for QorlQ LS series. Presented by Lidong Liu Presented at DwF Digital Networking - Nanjing - 21 May 2015 Session ID: APF-SNT-T1046
記事全体を表示
This session provides an introduction to the new QorIQ LS1 family, the first family of devices in the QorIQ LS series based on dual ARM® Cortex®-A7 cores. You will receive an overview of the LS1 processors--advantages, differentiators and capabilities for networking and industrial applications. Presented by You Peng Presented at DwF Digital Networking - Nanjing - 21 May 2015 Session ID: APF-SNT-T1358
記事全体を表示
This session will highlight the differences between the two architectures from the programming model, including overall architecture, instruction set architecture (ISA) and exception handling. After completion of this session, participants should have a good understanding of what is common and how to go about programming with devices based on ARM and Power Architecture technology. Presented by Satoshi Iida Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1043
記事全体を表示
Automotive and Connected Car Cost Efficient Solutions with Freescale Microcontollers for Automotive Applications Design, Software and Services Device Tree Made Easy Smart Home and Buildings Wireless and Connected Home of the Future Smart Industry Freescale's View of the Internet of Tomorrow Smart Networks Speed Your Time to Market by Leveraging Freescale’s Software, Tools and Professional Services for QorIQ Development Layerscape Use Cases Freescale Recommendations for Avionic and Defense Applications
記事全体を表示
For 20 years, Freescale has established networking IP and expertise with PowerQUICC and QorIQ processors based on Power Architecture®  technology. In this session, we will discuss the addition of the LS1 family of ARM®-based processors to the QorIQ portfolio and where we are growing the Power Architecture-based portfolio. We will also provide an update on the innovative Layerscape architecture platform and product roadmap for QorlQ LS series. Presented by Jim Bridgwater Presented at DwF Silicon Valley - March 26, 2015 Session ID: AMF-SNT-T1046
記事全体を表示