This article introduces the FreeMASTER blocks available in NXP Model-Based Design Toolbox (MBDT) and explains how they are used within a Simulink model to prepare an application for FreeMASTER integration.
The primary focus is the FreeMASTER Config block, which enables the FreeMASTER Driver in the generated application and allows users to configure the communication interface and runtime parameters required by FreeMASTER. The article also introduces the FreeMASTER Recorder block, which can be used to add data-recording capabilities to the application.
Before FreeMASTER can communicate with an embedded application, the FreeMASTER Driver should be enabled and configured in the embedded application. The FreeMASTER blocks provided by MBDT simplify this integration process by allowing all required settings to be configured directly within the Simulink environment.
This article is intended for:
By reading this article, you will understand how FreeMASTER support is enabled within a Simulink model and how the generated application is prepared for runtime communication and data access. You will also learn how the code-generation process produces an ELF file containing symbolic information corresponding to application variables, which is later used by FreeMASTER to access, monitor, and visualize application data.
Dedicated Simulink blocks integrate FreeMASTER into a Model-Based Design Toolbox project by automatically generating the software infrastructure required by the application.
The overall workflow is illustrated below:
Figure 1. FreeMASTER workflow
In this workflow, the FreeMASTER blocks serve as the interface between the Simulink model and the FreeMASTER Driver that will be included in the generated application.
FreeMASTER blocks can be found in the MBDT library under:
S32K3xx Core, System, Peripherals and Utilities → Utility Blocks
Figure 2. FreeMASTER Simulink Library
Three blocks are available for FreeMASTER integration:
The FreeMASTER Config block is responsible for enabling and configuring the FreeMASTER Driver within the generated application. It inserts the software infrastructure required for communication between the embedded target and the FreeMASTER desktop tool and serves as the foundation for integrating FreeMASTER functionality into a Simulink model.
Figure 3. FreeMASTER Config block
This block provides a configuration interface divided into two sections: communication settings and runtime settings.
The General tab contains communication-related parameters:
Figure 4. FreeMASTER General tab
During configuration, a dedicated communication peripheral is assigned to the FreeMASTER Driver. In the example shown, communication is performed through LPUART6 operating at 115200 bps.
The FreeMASTER Configuration tab contains runtime-related settings:
Figure 5. FreeMASTER Configuration tab
Together, these settings determine how the FreeMASTER Driver operates within the generated application.
In addition to the configuration block, MBDT provides a FreeMASTER Recorder block that enables support for FreeMASTER recording functionality.
Figure 6. FreeMASTER Recorder block
Unlike the Config block, which is primarily focused on communication setup and driver integration, the Recorder block is designed for high-speed monitoring and visualization of application variables. It configures data acquisition resources that can be accessed later through the FreeMASTER desktop application, enabling detailed analysis of system behavior.
The Recorder block is typically placed in application execution paths where rapidly changing signals need to be captured periodically. To support this, it uses an on-board memory buffer to store acquired samples, allowing high-frequency data to be recorded without requiring immediate transfer to the host PC. The buffered data can then be retrieved and displayed in FreeMASTER for waveform visualization, performance evaluation, and post-run analysis.
The block provides the following configuration parameters:
Figure 7. FreeMASTER Recorder block parameters
The Recorder block is optional and can be used whenever runtime data recording capabilities are required.
MBDT also provides a FreeMASTER Poll block, which allows the application to explicitly call the FreeMASTER polling function within the Simulink model.
Figure 8. FreeMASTER Poll block
The Poll block does not require any configuration parameters. Its purpose is to provide a configurable location within the application where FreeMASTER communication handling and command processing can be executed.
Figure 9. FreeMASTER Poll block mask
The role of the Poll block depends on the operating mode selected in the FreeMASTER Config block. When the FreeMASTER Driver is configured in Poll Mode, the Poll block is responsible for both communication handling and command processing. When the Driver operates in Short Interrupt Mode, communication is handled by interrupts, while command processing is performed through the Poll block.
When the FreeMASTER Driver is configured in Long Interrupt Mode, communication handling and command processing are performed entirely by the driver interrupt routines. In this configuration, the Poll block is not required, and its execution has no effect on FreeMASTER operation.
The Poll block complements the FreeMASTER Config and FreeMASTER Recorder blocks by providing a configurable mechanism for communication processing when required by the selected FreeMASTER operating mode.
Once the FreeMASTER blocks have been added and configured, the model can be built using the standard code-generation workflow provided by Embedded Coder and MBDT.
In addition to the application code generated from the Simulink model, the build process also produces an ELF (Executable and Linkable Format) file. When debug information is enabled during the build process, the ELF file contains symbolic information about application variables, functions, and memory locations stored in the DWARF debug sections. Otherwise, this information may be removed, preventing the FreeMASTER desktop tool from extracting the symbols required for variable access and monitoring.
The ELF file is later loaded by the FreeMASTER desktop tool, allowing variables to be identified automatically without requiring manual memory address entry. This enables features such as variable monitoring, runtime configuration, data visualization, and recording.
NXP_MBDToolbox_S32K3\FreeMASTER\
This article introduced the FreeMASTER Configuration blocks provided by NXP Model-Based Design Toolbox and explained their role in preparing a Simulink model for FreeMASTER integration. By configuring the block appropriately, developers can include the required FreeMASTER support in the generated application and produce an ELF file suitable for runtime access to application data.
The next article in this series will demonstrate how to use the generated application and ELF file to establish a connection between the target device and the FreeMASTER desktop application.