Toolbox workflow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Toolbox workflow

Toolbox workflow

1

Table of Contents


2

Introduction


This article provides a high-level overview of the typical workflow for developing an application using the toolbox. It explains how the main development stages fit together, from preparing the environment and selecting the target hardware to configuring the project, generating code, building the application, programming the target, and validating the results. The purpose of this topic is to help users understand the overall process and to guide them toward the related articles that describe each stage in more detail.

3

Overview


Workflow Scope

The workflow described in this article covers the main steps typically followed when developing an application with the toolbox. After the toolbox and supporting environment are prepared, the user can create a new model or open an existing example, select the target hardware, configure the required software components, prepare the Simulink model, generate code, build the application, program the target device, and debug and validate the behavior on hardware. This article is intended as an overview topic and does not replace the more detailed setup, modeling, and debugging documentation.

Target Audience

This article is intended for users who want to understand the overall development flow supported by the toolbox. It is useful both for new users who start from supported examples and evaluation boards and for advanced users who need to adapt the workflow to a custom target or project configuration.

4

Context


Prerequisites

Before following the workflow described in this article, the development environment should already be prepared. The setup process, including toolbox installation and the basic steps required to run an application, is described in the previous article. Depending on the selected project and application requirements, additional tools such as S32 Configuration Tools or EB tresos may be needed, especially when the default project configuration must be modified or when a custom project is created.

Toolbox Workflow

The development flow typically starts with creating a new project or opening an existing example and then selecting the target hardware.

image1.png

Figure 1. Opening a Simulink project or toolbox example.

The selected target determines the available peripherals, supported examples, software configuration options, and build settings. As part of this step, the user can start from the default project associated with the selected target. This default project provides a ready-to-use baseline configuration and is typically the recommended option for evaluation boards and quick start development. For more advanced use cases, the workflow can also use a custom project configuration adapted to the application requirements.

image2.png

Figure 2. Selecting a custom project configuration.

If the user continues with the default project configuration, additional low-level software changes may be limited. However, when the default project needs to be modified or when a custom project is used, tools such as S32 Configuration Tools or EB tresos may be required.

image3.png

Figure 3. Low-level software configuration using EB tresos or S32 Configuration Tool. image4.png

Figure 4. S32 Configuration Tool Configuration Template.

Once the software stack is prepared, the Simulink model must be configured. This includes adding and parameterizing the relevant toolbox blocks, defining the application behavior, setting the model parameters, and aligning the model with the selected target and software configuration.

image5.png

Figure 5. Embedded Coder.

image6.png

Figure 6. Build or Generate Code step.

After the model configuration is complete, code can be generated from the Simulink model. This step transforms the model into source code suitable for the selected target platform. The generated output reflects both the model behavior and the configuration settings applied in the previous stages.

The generated code is then built using a supported compiler toolchain. The build process compiles and links the generated code together with the required software components and libraries. Build settings may vary depending on the target, compiler version, and selected optimization or debug options.

image7.png

Figure 7. Generated code.

After a successful build, the application can be programmed onto the target hardware and executed. At this stage, the user can debug the application using the supported debug tools, inspect signals and variables, and verify that the application behaves as expected on the real hardware platform.

image8.png

Figure 8. Programming and debugging the application on target hardware.

The final step of the workflow is validation and iteration. If issues are found during testing or debugging, the user may need to update the model, adjust the low-level software configuration, or modify build settings. The workflow is therefore iterative, allowing repeated cycles of configuration, code generation, build, programming, and validation until the desired result is achieved.

Related Topics

Additional details for each workflow stage are available in related documentation topics. For environment preparation, toolbox setup, and the basic steps required to run an application, refer to the previous article. More detailed information about model creation and configuration is provided in the next article. Other related topics may include examples library, supported boards and derivatives, low-level software configuration, compiler versions and options, and debugger usage.

5

References


For more detailed information, refer to the related toolbox documentation and associated setup, modeling, software configuration, compiler, and debugging articles.

6

Conclusion


The toolbox workflow provides a structured path from model-based development to execution on the target hardware. Users can start quickly from the default project associated with the selected target, while still having the flexibility to create and use a custom project configuration when required. By following this workflow and using the related detailed documentation, users can iteratively configure, build, program, debug, and validate their applications more efficiently.

評価なし
バージョン履歴
最終更新日:
‎07-14-2026 02:39 AM
更新者: