Motor Control Class: GPIO PROGRAMMING

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Motor Control Class: GPIO PROGRAMMING

Motor Control Class: GPIO PROGRAMMING

This video shows how to program the GPIO with Model Based Design Toolbox to obtain the speed reference for the BLDC speed closed loop control system.

 

We discuss about:

- How to implement a simple program to read data from the GPIO

- How to test in real time with FreeMaster

- How to transform GPI pulses into a speed reference data that represents the rpm.

- How to implement from scratch a Simulink model to cover the GPIO functionality

NOTE: Chinese viewers can watch the video on YOUKU using this link.

注意:中国观众可以使用此链接观看YOUKU上的视频

ラベル(1)
コメント

Dear Dumitri,

I'm using Matalb Simulink v2017.b and the MBDT toolbox v2.0.0. Building project is successful, but I cannot succeed flashing the microcontroller (MPC5744P). The problem I identified is that I cannot change the COM port to download the code, in the Configuration Parameters > PIL and Download Config panel. Even if I type the correct number of COM port, the default value ('1') is kept.

Do you have any idea about the origin of the problem and how to fix it ?

Best regards

Alexandre Boyer

評価なし
バージョン履歴
最終更新日:
‎05-28-2017 09:40 PM
更新者: