Model-Based Design Toolbox for S12ZVMx Automotive Microprocessors Version 1.4.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Model-Based Design Toolbox for S12ZVMx Automotive Microprocessors Version 1.4.0

Model-Based Design Toolbox for S12ZVMx Automotive Microprocessors Version 1.4.0

 

 

 pastedImage_1.png

Product Release Announcement

Automotive Processing

 

NXP Model-Based Design Toolbox

 

for S12ZVMx – version 1.4.0

 

 

Austin, Texas, USA

September 9, 2020

The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S12ZVMx version 1.4.0. This release supports automatic code generation for S12ZVM peripherals and applications prototyping from MATLAB/Simulink for NXP S12ZVMx Automotive Microprocessors. This new release adds extended MATLAB version support (R2015a-R2020a), integrates with AMMCLib v1.1.21, is compatible with MathWorks Automotive Advisory Board checks, adds over 50 new examples and more.

 

FlexNet Location:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX

 

Activation link:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX

 

Technical Support:

NXP Model-Based Design Toolbox for S12ZVMx issues are tracked through NXP Model-Based Design Tools Community space.

https://community.nxp.com/community/mbdt

 

Release Content

  • Automatic C code generation from MATLAB® for NXP S12ZVMx derivatives:
    • S12ZVM 32/L31/16:
      • MC9S12ZVM16
      • MC9S12ZVML31
      • MC9S12ZVM32
    • S12ZVML/C 128/64/32:
      • MC9S12ZVML32
      • MC9S12ZVML64
      • MC9S12ZVMC64
      • MC9S12ZVML128
      • MC9S12ZVMC128
    • S12ZVMC256:
      • MC9S12ZVMC256

 

  • Integrates the Automotive Math and Motor Control Library release 1.1.21:

All functions in the Automotive Math and Motor Control Functions Library v1.1.21 are supported as blocks for simulation and embedded target code generation for:

  • Bit Accurate Model for 16-bit fixed-point implementation
  • Bit Accurate Model for 32-bit fixed-point implementation
  • Bit Accurate Model for floating-point single precision implementation

image.png

 
 
 
 
 
 

image.png

  • Extended support for MATLAB versions

We extended support for our toolbox to cover a wider range of MATLAB releases – starting from R2015a and going up to R2020a. This way we want to avoid locking out users that have constraints regarding MATLAB versions.

  • Motor control examples

We have added new motor control examples – BLDC (closed loop) and PMSM (closed loop, sensorless):

 

image.png

  • MAAB Checks (MathWorks Automotive Advisory Board)

The toolbox is compatible with MathWorks Automotive Advisory Board checks – reports can be generated from Model Advisor:

 

image.png

  • Updated examples:

We have added over 50 new examples, including:

  • Motor control (both BLDC and PMSM)
  • AMMCLib
  • GDU (Gate Drive Unit)
  • Profiler

For more details, features and how to use the new functionalities, please refer to the Release Notes document attached.

 

MATLAB® Integration

The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S12ZVMx MCUs and evaluation boards solutions out-of-the-box with:

image.png

Target Audience

This release (1.4.0) is intended for technology demonstration, evaluation purposes and prototyping S12ZVMx MCUs and Evaluation Boards.

 

Useful Resources

Examples, Trainings and Support: https://community.nxp.com/community/mbdt

 

 

 

 

 

                                          pastedImage_23.png

添付
評価なし
バージョン履歴
最終更新日:
‎09-24-2020 05:43 AM
更新者: