Model Based Design Toolbox Motor Control Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model Based Design Toolbox Motor Control Example

Model Based Design Toolbox Motor Control Example

This video shows:

- motor control typical setup with S32K144 rev2.0 Evaluation Board;

- Simulink model for a BLDC motor control;

- how to setup Simulink to generate ANSI C code for S32K144 rev2.0 MCU;

- quick tour of the Model Based Design Toolbox;

- quick tour of the FreeMASTER data visualizer;

- Motor Control example running with DevKit S32K144EVB and MotorGD shield;

(view in My Videos)
Labels (1)
Comments

Thanks for sharing, but where is the C code?

Hello fuyanchao@protonmail.com‌,

The Simulink generates and builds automatically the C code so the user don;t need to interact with the C code. If the user wants to see/debug the C Code, this is available in a folder next to the Simulink Model.

If you are asking about the model presented in this video, please download and install our toolbox and you will find the model there.

Hope this helps,

Marius

Thank you very much!

No ratings
Version history
Last update:
‎04-28-2017 02:02 AM
Updated by: