Developing a Parking Sensor System with Model-Based Design Toolbox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Developing a Parking Sensor System with Model-Based Design Toolbox

Developing a Parking Sensor System with Model-Based Design Toolbox

 

1

Table of Contents


2

Introduction


Parking assistance systems are a familiar feature in modern vehicles, helping drivers detect nearby obstacles and maneuver the vehicle more safely. In our Hello World with MBDT project, the parking sensor subsystem provides this capability by measuring the distance to nearby objects and supplying that information to the rest of the system.

Figure 1 - Physical concept.pngFigure 1 - Physical concept.png

Figure 1 - Physical concept

This article introduces the parking sensor system and leads into the next articles in the series, where we will examine how this part of the project is developed. The Parking Sensors System (PSS) focus is set on how Model‑Based Design (MBD) enables the subsystem to be designed, simulated, tested, and deployed rapidly using MATLAB/Simulink and the NXP Model-Based Design Toolbox (MBDT).

 

3

Overview


The role of this subsystem within the overall project describes the main elements that make up the parking sensor application and explains its purpose and behavior at a conceptual level. The article outlines how NXP's MBDT supports the development of this component and how a single model is reused for both front and rear parking modules. It also clarifies how this component fits into the larger project and how it connects to the rest of the components.

The importance of this subsystem lies not only in its functional role of acquiring and processing distance information but also in how it demonstrates the efficiency of model‑based workflows. Rather than relying on traditional hand‑written embedded code, the entire application — logic, algorithms, peripheral drivers, timing behavior — can be designed graphically in Simulink.

This accelerates development in several ways:

  • Behavior can be simulated on the PC, without flashing hardware.
  • The same model drives both simulation and embedded implementation.
  • Peripheral interactions like Analog‑to‑Digital Converter (ADC) and Local Interconnect Network (LIN) are handled through dedicated blocks, not hand‑written code.
  • Parameter tuning and validation are simplified through FreeMASTER, providing real-time visualization of the embedded system parameters.
  • This accelerates development and ensures that the final embedded behavior matches the tested model.

Developing an embedded sensor node application typically involves writing extensive low‑level code, configuring peripherals manually, and iterating slowly through hardware tests. This slows down development, limits experimentation, and creates fragmentation between design and implementation.

The parking sensor subsystem demonstrates how Model-Based Design in Simulink solves this problem by enabling the entire feature to be built directly in Simulink. Engineers can model ADC acquisition, LIN communication, filtering logic, and threshold detection using graphical blocks rather than manual code. They can simulate the behavior instantly, refine algorithms quickly, and deploy the design to the microcontroller through automatic code generation.

The MBD approach significantly improves the efficiency and reliability of developing, testing, and refining the complete parking sensor application.

This series is intended for:

  • Engineers learning Model‑Based Design with MATLAB/Simulink
  • Developers working with NXP automotive microcontrollers
  • Teams building rapid prototypes of embedded measurement and control features
  • Students and researchers studying vehicle architectures
  • Anyone interested in a full, reproducible example of embedded system development using MBDT

Readers will gain a clear, step‑by‑step understanding of how a complete embedded feature is designed and implemented using a unified model‑based workflow.

 

4

Context


A key aspect of the design is that the same PSS application developed in Simulink is used for both front and rear parking. Two separate S32K144 boards run the identical autogenerated code — one at the front of the vehicle and one at the rear. This showcases one of the major advantages of MBD: a single validated model can be scaled, cloned, and reused across multiple hardware nodes with minimal parametrization.

Figure 2 - Parking System Architecture.pngFigure 2 - Parking System Architecture.png

Figure 2 - Parking System Architecture

The purpose of the parking sensor subsystem is to provide a clean, consistent, and rapidly developed interface that delivers accurate distance information to the rest of the system.

In the implemented setup, each ultrasonic sensor outputs an analog voltage proportional to distance. This signal is sampled by the ADC (Analog‑to‑Digital Converter) of the S32K144 microcontroller. The embedded application running on the S32K144 performs the acquisition sequence, processes the ADC values to compute distance measurements, and formats the results into a communication frame. The prepared data is then transmitted over the LIN bus to the zonal controller, where it can be further used by higher‑level vehicle functions.

All functional aspects — ADC acquisition configuration, signal processing, communication formatting, and diagnostic handling — are defined directly in the Simulink model, enabling rapid refinement and immediate validation through simulation. During development, FreeMASTER is used to monitor live ADC samples from the ultrasonic sensors, observe processed distance values, and validate the behavior of the embedded application before integrating the component into the full system.

The parking sensor component (front and rear) is highlighted to show its position in the project setup:

Figure 3 - Parking System highlighted within the project.pngFigure 3 - Parking System highlighted within the project.png

Figure 3 - Parking System highlighted within the project

Related articles in the series

Note: Additional articles in the series, including topics such as Software & Hardware Environment, Architecture & Model Description, Deploy & Validate on Hardware, Final Results and Challenges, will be added here as they become available. Each will explore individual technical details such as ADC acquisition, model structure, filtering logic, and communication behavior introduced in this overview.

 

 

6

Conclusion


The parking sensor subsystem demonstrates how Model-Based Design accelerates the development of embedded automotive features. By modeling the sensing logic in Simulink, validating behavior through simulation, downloading it automatically using MBDT and monitoring it on hardware with FreeMASTER, the entire application can be developed and deployed from within a single environment. Rather than duplicating the parking sensors logic, the application is implemented as a parameterized Simulink model. Using MBDT, the same model instance can be configured for the front or rear module by adjusting parameters such as communication identifiers. This approach enables consistent behavior across parking modules while minimizing duplication and simplifying maintenance.

This article introduced the component's behavior, purpose, and development workflow. The next articles in the series will expand on specific technical aspects, building a complete understanding of the subsystem from model to deployment.

无评分
版本历史
最后更新:
‎07-23-2026 04:34 AM
更新人: