NXP FTF 2016 - 培训演示

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP FTF 2016 - Training Presentations

讨论

排序依据:
This session will cover the different vision processing capabilities of the S32V234 automotive vision processor with a focus on the Image Sensor Processor (ISP). The presentation will demonstrate how the cost of a vision system can be cut down by using the ISP to accept raw camera input data and to process it using algorithms like debayering, white balancing, format conversion, HDR and de-noising. The aim of the session is to give an introduction to camera processing, to present the architecture of the ISP and to demonstrate how it can be programmed using a visual tool developed by NXP.
查看全文
When adapting Android to a custom product, system updates are a very important matter. Fortunately Android provides a reliable update mechanism which can also be customized to your needs. Learn how to use it and/or implement some customizations from the recovery image to the OTA client application. A demonstration will be featured showing different use cases on i.MX6-based hardware.
查看全文
Multi-Core Embedded Frameworks are increasingly being used on NXP hardware to host RTOS, Linux and other proprietary operating systems. When it comes to debug, new tools are needed to allow step-by-step time-synchronized debug of individual cores, and their role in the overall system performance. This paper looks at Mentor Embedded Codebench, and the Sourcery Analyzer design debug options.
查看全文
We will show you how to use and leverage the work done by NXP's board solutions team to increase quality, reduce design iterations, decrease costs, and reduce time to market. NXP has extensive manufacturing expertise and can provide guidelines and advice on symbols and footprints as well as product development challenges. NXP maintains a qualified library of parts to reduce costs and promote common components. Using a proven design process will help to reduce board spins and development time. Schematic standards will improve overall quality and taking advantage of design reuse will reduce cycle time. Watch Video Presentation
查看全文
With the introduction of MIFARE Plus® EV1 NXP enables universities currently using MIFARE Classic to introduce latest technology in the existing system, upgrade the security of applications depending on their needs and complement daily use cases with mobile devices. Through the option to upgrade individual applications of your system fast security upgrades for critical applications are possible whereas non-critical applications remain in the existing mode without any changes. MIFARE Plus EV1 further includes the option to complement existing applications with mobile use cases. Through its enhanced possibilities MIFARE Plus EV1 based cards can now easily be integrated in cloud applications while maintain banking grade security.
查看全文
Embedded Planet designed the new NXP LS1043 Gateway. Come learn the details of the hardware and software designed for this next generation residential Gateway.
查看全文
Gain a deep dive into the GPU and display controller architecture of the i.MX 8 applications processor family. Discover the advanced features, design choices, and the HMI solutions enabled by the i.MX 8 series. This class provides a basic introduction to i.MX 8 graphics and is a precursor to the more advanced i.MX 8 classes around augmented reality, eCockpit, graphics SDK and Vulkan classes. Watch Video Presentation
查看全文
Using Accelerometers, Magnetometers, Gyroscopes, gathering Sensor data can be tricky and not straight-forward. In this class, we will go into a Sensor Deep-Dive, where each sensor will be visualized and explained in detail. When collecting data there are several things that can make collecting the data easier, more efficient, and avoiding erroneous data all together. We will have several demonstrations and examples to show the pitfalls and successes of collecting data.
查看全文
This paper will examine the use of an i.MX 6 IOT Gateway working together with a Cloud Services Platform (CSP), to collect and transmit data from a temperature sensor. The design options for seamless data transmission from device, to gateway, to cloud and then to a hand-held Smartphone will be considered and presented using Mentor Embedded Linux, Nucleus as well as Cloud Service Platforms.
查看全文
This session will provide an overview of the QorIQ's hardware root of trust, key protection, and strong partitioning capabilities. Watch Video Presentation
查看全文
FIDO Alliance is getting huge traction in the secure authentication world and the member count has surpassed 250 companies. Secure Element based FIDO U2F Authenticators add another security layer to consumer online authentication for cloud services and have been deployed for services like Google, Dropbox, Github, and others. These Authenticators are available in various form factors (Cards, USB keys, Fobs, Wearables and embedded) and support multiple interfaces like USB, NFC and BLE to connect users to critical online services using the FIDO authentication protocol. In addition to FIDO credentials, NXP provides vSE based multi-credential (PKCS#15, EAC, BAC, SAC, Mifare, PIV ) as well as an online services platform including eDoc derived mobile credential management connecting relying parties to enable secure mobile authentication for eGov services. Watch Video Presentation
查看全文
Transport ticketing requirements have evolved significantly over the last years - from transaction security to multi-application needs and the possibility to integrate mobile ticketing to an existing environment. NXP's MIFARE® products have consistently been able to meet these requirements and strongly establish an excellent reputation as the leading contactless solution delivering convenience, flexibility and scalability. Over 1,000 business partners including application developers, service and solution providers, system integrators and card manufacturers make up the open MIFARE community and ecosystem. MIFARE DESFire EV2 is the next-generation of MIFARE ICs with highest security level (EAL5+ Common Criteria certification) for hardware and software. Its enhanced key management makes it the ideal multi-application platform for unlimited applications.
查看全文
ODP and DPDK are open-source project that defines a standard set of APIs for data-plane to be used across the different network processor architectures. This session details how the standard DPDK and ODP APIs are being mapped to NXP data-path acceleration for specific packet processing elements (packet IO, classification, scheduling, crypto, etc.). It also propose various possible API extensions to get additional performance on NXP SoCS. This presentation will cover how the ODP and DPDK can provide the necessary infrastructure for virtualized environments.
查看全文
Smart digitalized packaging as a subset of the Internet of Things - a huge trend impacting global packaging industry today. NXP is the Identification industry's #1 chip supplier for smart secure NFC-RFID technology offering a variety of tag ICs from short to long-range, allowing interaction with mobile phones connecting products to the cloud and customers to brands. Watch Video Presentation
查看全文
This session will provide tips that will help speed up silicon bring up of the QorIQ LS1043A processor.
查看全文
The session will provide an overview of the most recent developments to support Radar systems in the frequency range from 76 GHz up to 81 GHz. High level block diagrams and key specifications of NXP multi-channel transceivers will be presented. It will also be discussed how the NXP transceiver solutions can help to enable modern low power consumption sensors with robustness against frequency interference, small size, and high-performance due to scalability. In combination with NXP Radar micro-processors and mircro-controllers typical Radar system architectures will be introduced. Especially for the development of small and compact cocoon, nano radar sensors an example is presented which shows the combinations of NXP Radar tranceivers, NXP Radar processors and NXP power supply solutions. The presentation will also give an outlook to technology trends and future upcoming NXP Radar solutions.
查看全文
The AIOP C programmable packet engine is a fundamental component of the Data Path Acceleration Architecture (DPAA2). It provides customers with an opportunity to achieve the best performance per watt solution, by offloading routine packet processing tasks to the AIOP packet engine, while doing more complex processing on the ARMv8 cores. This sessions explores how customers can get to fast time-to-market with high performance, commercial grade acceleration packages from NXP.
查看全文
Building on top of 11 years of usage within data centers, Xen Hypervisor is uniquely placed to support a new range of use cases for embedded solutions. In particular, its isolation and security features, flexible virtualization modes and architecture, driver disaggregation, and strong ARM support make it a perfect fit for embedded applications. Artem Mygaiev, GlobalLogic’s Embedded Practice Head, will explore the virtualization nuances and challenges of using Xen Hypervisor for embedded applications through the demonstration of his own company’s journey in developing a platform that leverages Xen for virtual network equipment, IoT, automotive, and other embedded use cases.
查看全文
Networking devices use high-speed differential signaling that can exceed 10 Gbps. Circuit design for the transmitter (TX) and receiver (RX) elements in the high speed channel have capabilities of offset signal losses in the PCB and system. This session will review the high-speed signal channel and its characteristics and illustrate how the TX and RX circuits in general are used to offset signal losses. It will also show key characteristics of the channels that are needed to allow these TX and RX circuits to work effectively. This session will also address maximum length of the PCB channel, PCB-specific structures that need to be optimized and the usage of the IBIS-AMI models for 5-10 Gbps operation. Examples of channels from PCB designs at NXP will also be included. Watch Video Presentation
查看全文
Cars depend on a range of systems that must guarantee safety for their drivers. Linux and Open Source have already entered the infotainment segment, but expanding to ADAS presents new challenges with regards to safety and change control. This session will provide an overview of the internals of the kernel, the safety-critical components, implementation of fault recovery mechanisms and finally how open source software can be used for Autonomous Drive applications. Watch Video Presentation
查看全文