filter within the product selector

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

filter within the product selector

2,496 Views
eric_langner
Contributor I

Hello,

I`d like to have some support because the product selector does not fit to my needs.

I`d like to filter out (within all the processors and microcontroller list) by

a) camera interface 

b) FlexIO

c) MIPI CSI-2

(perhaps also with IPU) in the first step. Is this somehow possible ?

Cheers and thank you !

Tags (1)
0 Kudos
Reply
3 Replies

2,433 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello Eric,

Thank you for the opportunity to work with you.

In the Product Selector you can look for an MPU that has MIPI CSI-2. Here is a link of the product selector to start with:

Product Selector | NXP 

Please, If you could give us a little more info about the usage of the FLEXIO I can recommend a specific MPU.

If you check on the side-bar in the Camera Interfaces option, you will see the MIPI-CS-2 option. Unfortunately 
Have a great day,
Fabian

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Best Regards,
Fabian
0 Kudos
Reply

2,433 Views
eric_langner
Contributor I

Hello Fabian,

thanks for your reply. I`m looking or an MCU\MPU with the following parameters. 

+ FlexIO or camera I/F

+ approx. 512KB Flash (min. 256KB)

+ approx. 256KB SRAM (under certain circumstances 128KB would be also okay)

+ USB is a must have

+ max. 7 USD

What I found s far ist: K32 L3 / K32 L2A / KL2x / K8x / Crossover-RT1050 / Crossover-RT1015 / Crossover_RT1010. Would you recommend one of these or another one for a new design ? I`m more interested for an platform with camera I/F (or FlexIO) than MIPI CSI-2. 

Have a great day, Eric

0 Kudos
Reply

2,433 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello Eric,

I recommend i.MX RT1064 crossover MCU| Arm Cortex-M7| NXP | NXP, This crossover-MCU has the camera I/F you are looking for, along with 4Mb on-chip flash memory, 1Mb SRAM and 2 USB-PHY. So I think this fits perfectly with your project.


Have a great day,
Fabian

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Best Regards,
Fabian
0 Kudos
Reply