The installation of S32 Design Studio for Power Architecture Version V2.1 has been rolled back.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The installation of S32 Design Studio for Power Architecture Version V2.1 has been rolled back.

3,248 Views
marco_li
Contributor I

The installation of S32 Design Studio for Power Architecture Version V2.1 has been rolled back.

The attached file is the installation log.

Labels (1)
0 Kudos
Reply
3 Replies

2,371 Views
Hwanmin
Contributor II

Hello.

Could you tell me how to check the access? I'm having the same problem. Thank you.

0 Kudos
Reply

3,104 Views
marco_li
Contributor I

The screenshot is as below:

pastedImage_1.png

0 Kudos
Reply

3,104 Views
mikedoidge
NXP Employee
NXP Employee

Hello marco.li@zongmutech.com‌,

In the installation instructions, it is stated that the user must have administrative access when installing S32 Design Studio for Power Architecture. Without this, there will be access denials during installation which will trigger the rollback. This is seen in the log file provided:

Install Uninstaller: S32 Design Studio for Power Architecture Version 2.1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Could you please confirm if the tool was installed with administrative access enabled?

Best Regards,

Mike

0 Kudos
Reply