Synchronous Abort Issue S32V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Synchronous Abort Issue S32V

2,396件の閲覧回数
hfahema
Contributor I

I am receiving this error message here when trying to boot an S32V234 from an SD card.

U-Boot 2016.01+g4627170 (May 22 2019 - 12:48:54 -0700)

CPU: NXP S32V234 V2.0 at 1000 MHz
Reset cause: Software Functional reset
Board: s32v234bbmini
I2C: ready
DRAM: "Synchronous Abort" handler, esr 0x96000010
ELR: 3e828200
LR: 3e84816c
x0 : 000000007fd7af68 x1 : 000000003e856832
x2 : 0000000080000000 x3 : 000000003e8281ec
x4 : 000000007fd7b000 x5 : 0000000000000013
x6 : 0000000000000098 x7 : 0000000020000000
x8 : 00000000fffff7ff x9 : 000000000000000c
x10: 00000000feeff7ff x11: 000000003ebdfa8d
x12: 00000000ffffffff x13: 00000000ffffffff
x14: 0000000080000000 x15: 0000000080010000
x16: 000000003e822530 x17: 2114214011001432
x18: 000000003ebdfca0 x19: 000000003e85e0f0
x20: 000000003e85dfe8 x21: 0000000000000000
x22: 042401a8bf30080e x23: ff980013008de800
x24: 0c01310935d14c10 x25: 3002101258802340
x26: 45098e49014f1628 x27: b00005020a90b602
x28: 498aa85c99a10024 x29: 000000003ebdfc50

Resetting CPU ...

resetting ...


U-Boot 2016.01+g4627170 (May 22 2019 - 12:48:54 -0700)

CPU: NXP S32V234 V2.0 at 1000 MHz
Reset cause: Software Functional reset
Board: s32v234bbmini
I2C: ready
DRAM: "Synchronous Abort" handler, esr 0x96000010
ELR: 3e828200
LR: 3e84816c
x0 : 000000007fd6af68 x1 : 000000003e856832
x2 : 0000000080000000 x3 : 000000003e8281ec
x4 : 000000007fd6b000 x5 : 0000000000000013
x6 : 0000000000000098 x7 : 0000000020000000
x8 : 00000000fffffffd x9 : 000000000000000c
x10: 00000000ffeffffd x11: 000000003ebdfa8d
x12: 00000000ffffffff x13: 00000000ffffffff
x14: 0000000080000000 x15: 0000000080010000
x16: 000000003e822530 x17: 2114214011001432
x18: 000000003ebdfca0 x19: 000000003e85e0f0
x20: 000000003e85dfe8 x21: 0000000000000000
x22: 042401a8bf30080e x23: ff980013008de800
x24: 0c01310935d14c10 x25: 3002101258802340
x26: 45098e49014f1628 x27: b00005020a90b602
x28: 498aa85c99a10024 x29: 000000003ebdfc50

Resetting CPU ...

This error continues repeating indefinitely. I am asking for help from the NXP community about how to interpret this error and also possible reasons for this error. I believe this error can either be coming from a corrupted SD card or compromised communication to the DDR3 chips.

I can provide more information upon request. Thank you for the help!#@

ラベル(1)
0 件の賞賛
返信
0 返答(返信)