SJA1105 can be used between two mcu?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1105 can be used between two mcu?

2,325 Views
caolejun
Contributor I

Hello,

My Pcb has two MCU:S32V234 and TC297. If I use a SJA1105 to connect this two mcu, is it OK?

0 Kudos
Reply
3 Replies

2,250 Views
Bulat
NXP Employee
NXP Employee

Yes, it is ok.

Regards,

Bulat

0 Kudos
Reply

2,250 Views
caolejun
Contributor I

Thank you Bulat Karymov!

So I chose TC297 to control SJA1105 by SPI,then in my code:

1. Should TC297 initialize SJA1105 first?

2. S32v need initialize SJA1105?

Thanks! 

0 Kudos
Reply

2,250 Views
Bulat
NXP Employee
NXP Employee

The SJA1105 is configured via SPI, so it should be configured by the controller with SPI connection to the switch.

Regards,

Bulat

0 Kudos
Reply