RFU bits in the EEPROM for PN5180

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RFU bits in the EEPROM for PN5180

3,562 Views
Shio_Tamba
Contributor II

 

Hi,

 

I have a question about RFU bits in the EEPROM for PN5180.

 - If you will use RFU bits in the EEPROM, the characteristic number(e.g. FW version, EEPROM version etc.) will change ?

 

Sincerely,

 

Tags (2)
0 Kudos
Reply
3 Replies

3,551 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @Shio_Tamba ,

 

Actually these addresses are read only, so would not change them at all.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,530 Views
Shio_Tamba
Contributor II

 

Hi,

 

- Actually these addresses are read only, so would not change them at all.

This fact is already understanding.

I think that the RFU bits will use for the future function of the PN5180. (because RFU = reserved for future use.) 

I guess that when you(NXP) assign the function to RFU bits, the specification numbers (e.g. FW version, EEPROM version etc.) will change of the PN5180 chip.

This is correct?

 

Sincerely, 

0 Kudos
Reply

3,500 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @Shio_Tamba ,

 

Well, from my understanding, when RFU bits have a new definition, the firmware should also be updated.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply