PTN3460 LVDS Bridge - Emulation Disabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3460 LVDS Bridge - Emulation Disabled

5,607 Views
pauldemet
Contributor I

Does anybody have experience using the PTN3460 device with emulation mode disabled?

Trying to use this mode but cannot get any display on the panel. Have not verified EDID data being retrieved from the panel on the DDC bus yet.

Where does EDID data retrieved from a panel reside on the bridge device? Is it accessible or visible?

The only change made to the registers is to clear the 'Enable EDID emulation' bit in the EDID ROM emulation control register.

0 Kudos
Reply
4 Replies

5,552 Views
pauldemet
Contributor I

I believe I got this working now. Needed to add the flash memory step found on page 10.

The flow diagram does not show any delay between emulation mode being disabled and the flash memory sequence. I would expect some kind of delay for the EDID table to be retrieved from the panel.

I added a 3 second delay but would like to know what is required?

 

0 Kudos
Reply

5,562 Views
pauldemet
Contributor I

I am already doing this as stated in the original message. Is this all that needs to be done?

Any debug hints would be helpful.

0 Kudos
Reply

5,564 Views
guoweisun
NXP TechSupport
NXP TechSupport

Suggest you follow the app note attached from page8-PTN3460 is in EDID emulation off mode (Configuration register 0x84 bit 0
= 0)

0 Kudos
Reply

5,238 Views
pauldemet
Contributor I

IS the EDID table read from the panel accessible? Can I read back the EDID table?

0 Kudos
Reply